![]() |
|
||||||
|
|
|
For more information:
Media contact: Amanda Summers, Vishay Measurements Group phone + 44 (0) 29 2055 5093 fax + 44 2079 00 22 98 e-mail amanda.summers@vishay.com Technical contact: David Viney, Nobel Ltd. phone + 44 (125) 646 2131 fax + 44 (125) 647 1441 e-mail David.Viney@vishaymg.com Vishay Nobel P9420 Series of Pressure Transmitters Provides Range Up to 15,000 psi (0 - 1,000 bar) and Secondary-Containment Option Up to 22,500 psiCombined error due to non-linearity, hysteresis, and repeatability is better than 0.25% FSO, while stability is better than 0.1% FSO per yearMALVERN, PENNSYLVANIA March 30, 2005 Vishay Intertechnology, Inc. (NYSE: VSH) announces the availability of Vishay Nobel P9420-800 series pressure transmitters. A further development in the range of hammer-lug union fittings for the offshore oil industry, the P9420-800 series pressure transmitters are an extension of the P9420 series with fused ceramic sensors that provide high shock and vibration immunity. All ranges of these transmitters are built within a male sub-casing, offering optional secondary containment of pressure up to the proof rating of the union assembly. The P9420-800 transmitters are available with a two-year warranty, and wide variety of connector options to suit the application requirement. Construction is of ultra-rugged stainless steel. These transmitters range up to 15,000 psi (0 - 1,000 bar) and the secondary-containment option is up to 22,500 psi. Combined error, non-linearity, hysteresis, and repeatability accuracy is better than 0.25% FSO, while stability is better than 0.1% FSO per year. Output is 4-mA to 20-mA, two-wire. The transmitters have ATEX and are also tested to IEC 68 Test Ea100g/6ms, 3 axes and Test Fc 10-800Hz, 5g, 3 axes for shock and vibration. They conform to IP68 BS5490:1977 and IEC 529:1976 and are tested to IEC 801-3 Parts 2,3,4 and 6 EN 50082-2 for RFI/EMC immunity. Vishay Nobel, which specializes in the design and manufacture of industrial weighing, force, and pressure measurement systems, has over thirty years of experience in designing and supplying systems for worldwide markets. The product range includes load cells, force and pressure transducers, instrumentation (such as indicators and transmitters), and application software. Vishay Nobel is part of the Vishay Transducers division of Vishay Measurements Group. Vishay Measurements Group develops, manufactures, and markets a broad range of sensors for a wide variety of test and measurement applications. These include electrical resistance strain gages for both stress analysis testing and transducer manufacturing applications, instrumentation, hybrid strain gage assemblies and transducers for OEM applications and certified load cells for electronic scales and other weighing applications. Vishay Measurements Group is part of Vishay Intertechnology. Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com. ###
| ![]() | ||||
![]() |
|||||
| ||||||