English   日本語 (Japanese)   简体中文 (Chinese)   
VishayOne of the world's largest manufacturers of discrete semiconductors and passive components
Vishay ProductsVishay ProductsCompany InfoApplicationsCompany Info
Company Info:Press Room:2005 Releases:New Low-Capacitance ESD Protection Diode Arrays
For more information:
Media contact:  E-mail:  bob.decker@wallstcom.com
Sales contact:  http://www.vishay.com/diodes/protection-tvs-esd/sales
 

Vishay's New Low-Capacitance ESD Protection Diode Arrays Provide High Standard of Protection in Compact 2.0-mm by 2.0-mm and 1.6-mm by 1.6-mm SMD Packages

MALVERN, PENNSYLVANIA — June 17, 2005 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced the release of two new Vishay Semiconductors low-capacitance ESD protection diode arrays that extend the company's line of ultra-small LLP-packaged products optimized for data-line protection in compact portable electronics.

The VESD05A8-HN2, packaged in the 2.0-mm by 2.0 mm LLP70 9A, features nine contact pads and a monolithic die with eight protection diodes - a quantity of diodes that until now was available only in the much larger 5.0 mm by 5.0 mm SO-8 package. As a result, the new array provides bidirectional asymmetrical (BiAs) protection for eight data lines, or bidirectional symmetrical (BiSy) protection for seven data lines.

The new VESD05A6-HA3 is packaged in the exceptionally small 1.6-mm by 1.6-mm LLP75-7A and features seven contact pads and a monolithic die with six protection diodes. The array offers bidirectional asymmetrical (BiAs) protection for six data lines or bidirectional symmetrical (BiSy) protection for five data lines.

The new leadless SMD arrays meet a high industry standard for ESD protection, supplying transient protection of 30 kV (air) and 30 kV (contact) as per IEC 61000-4-2, as well as 5-A protection against lightning as per IEC 61000-4-5. Their low capacitance minimizes distortion to the operating signal on protected lines.

In protecting very sensitive mobile electronics - such as mobile phone handsets, smart phones, laptop computers, PDAs, digital cameras, and MP3 players - against electronic discharge pulses caused by user contact with displays and keypads, the VESD05A8-HN2 and VESD05A6-HA3 also protect power supply and data transfer connections against discharge spikes. The devices' superior protection capability in a single compact package not only saves space, enabling design of smaller and/or more robust electronics, but also reduces manufacturers' component costs.

Sample quantities of the new VESD05A6-HA3 and VESD05A8-HN2 ESD protection arrays are available now. Production quantities with lead times of 8 to 12 weeks for larger orders will be available in late Q2 2005 for the VESD05A6-HA3 and late Q3 for the VESD05A8-HN2.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

 
Diodes
 

Products mentioned

 

This release in:

About Vishay
Brands
Careers
Contacts
Ethics
Investor Relations
Product News
2010 releases
2009 releases
2008 releases
2007 releases
2006 releases
2005 releases
2004 releases
*2003 releases
*2002 releases
*2001 releases
*2000 releases
*1999 releases
Terms and Conditions of Sale
Trade Shows
Vishay History
Products A-Z
Company Info:   Press ·  Investors ·  Contacts ·  More...
Privacy & Legal · Your Account