Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

New Vishay Siliconix 1-A Protected High-Side Load Switch in SOT-23 and SC-70 Packages Provides User Selectable Current Limit for Sub-5.5-V Applications


Load Switch

Products mentioned:

SiP4610A/B
For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

This release in:

MALVERN, Pa. — July 25, 2005 — Vishay Intertechnology, Inc. (NYSE: VSH), today announced a new protected high-side load switch that can operate under a supply voltage range of 2.4 V to 5.5 V and handle a continuous output current of 1 A, with the threshold current set by a single external resistor.

The SiP4610A/B is designed for applications including load switching, battery switching, USB peripheral ports, and other power management applications in notebook computers, PDAs, MP3 players, and other portable and handheld systems, as well as for hot-swapping in telecom applications.

A user-defined current limit level protects the input supply voltage from excessive load currents that might cause a system failure. The SiP4610A/B has a low quiescent current of 9 μA, and reduces the supply current to less than 1 μA in shutdown mode.

In addition to the current limit, the SiP4610A/B is protected by undervoltage lockout and thermal shutdown features. The over-temperature protection circuit prevents thermal runaway by turning off the power switch when the chip’s junction temperature reaches 165 °C and leaving it off until the temperature drops below 145 °C.

Providing the ability to selectively turn on and shut down various system functions, and to switch between power supply sources, there are two versions of the power switch. The SiP4610A has an active low enable input, while the SiP4610B has an active high enable input.

Available in lead (Pb)-free 5-pin SC-70 and thin SOT-23 packages, the SiP4610A/B operates within the industrial temperature range of -40 °C to 85 °C. It provides circuit designers with a pin-for-pin replacement for the AAT4610A.

The SiP4610A/B complements the wide range of Vishay Siliconix power switching products, which include the Si4701BDY (7 A) load switch with level-shift and the LITTLE FOOT® Plus families of power MOSFETs with integrated drivers and Schottky diodes (430 mA to 13.5 A).

Samples and production quantities of the new SiP4610A/B power switch are available now, with lead times of six to eight weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

LITTLE FOOT is a registered trademark of Siliconix incorporated

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword