|
For more information: Vishay's New SuperTan® Extended-Range Capacitors OfferIndustry-High 6000 Microfarad Capacitance in Standard T4 Package
MALVERN, PENNSYLVANIA — July 29, 2005 — In a breakthrough for wet tantalum capacitor technology, Vishay Intertechnology, Inc. (NYSE: VSH) today announced additions to the SuperTan® family of wet tantalum capacitors that include a device with the highest capacitance value yet achieved in the standard T4 package. With a rugged, all-tantalum construction, the new SuperTan Extended (STE) capacitors provide reliable performance in low-voltage filtering and energy storage applications for demanding, high-stress military and aerospace systems including weapon systems, radars, transponders, and power supplies. STE capacitors combine the inherent reliability of wet tantalum capacitors with the capacitance stability of solid tantalum to eliminate circuit impedance restrictions and dramatically increase capacitance ratings. A unique cathode system used in these SuperTan devices provides the highest capacitance-per-unit volume available on the market. The hermetically sealed, extended-range STE devices are available in industry-standard T1, T2, T3, and T4 case sizes. In the T4 case size measuring 1.062 in. [26.97 mm] long and 0.375 in. [9.53 mm] in diameter, the new device features capacitance ratings of 750 μF at 75 V and 6000 μF at 16 V - ratings that are up to six times greater than those of conventional wet tantalum products. By providing designers with a new high standard for capacitance in a single device, the new STE capacitors enable reduction of capacitor or component count, lower the amount of board space required, and simplify the overall manufacturing and assembly process. STE capacitors are capable of withstanding a 2,000-hour life test at a temperature of +85 °C at the applicable rated dc working voltage. Capacitance tolerance at 120 Hz and +25 °C is ±20%, with ±10% available upon request. The devices' operating temperature range is -55 °C to +85 °C. This may be extended to +125 °C with proper derating. Samples and production quantities of the new SuperTan capacitors are available now, with a lead time of 8 to 10 weeks for larger orders.
Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com. |