VishayOne of the world's largest manufacturers of discrete semiconductors and passive components
Vishay ProductsVishay ProductsCompany InfoCompany InfoCompany Info
Company Info:Press Room:2005 Releases:Vishay Siliconix LDO Regulator
For more information:
Media contact: e-mail bob.decker@wallstcom.com
Sales contact: http://www.vishay.com/power-ics/sales
 

Vishay Siliconix LDO Regulator Combines Low 130-mV Dropout with High 150-mA Current in SC-70 Package

MALVERN, Pa. — August 1, 2005 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced two new 150-mA low-noise low-dropout (LDO) regulators with the highest available current density in the small five-pin SC-70 package. Their extremely small 2-mm by 2-mm footprint makes them well suited for use in battery-powered equipment such as cell phones, PDAs, pagers, digital cameras, MP3 players, cable and DSL modems, and other noise-sensitive electronics.

Under a 150-mA load condition, the SiP21101 and SiP21102 feature an extraordinarily low dropout of 130 mV and a ground current of 110 µA, helping to prolong battery life in low-voltage portable electronic systems. Designed to maintain regulation while delivering 300-mA peak current, the new ICs both feature a fast start-up time of 50 µs, making them an excellent choice for systems that have a high surge current upon turn-on. Fifteen fixed output voltage options ranging from 1.2 V to 5.0 V are available.

The SiP21101 can be used as pin-for-pin replacement, with significantly improved current handling, for the MAX8510 and MIC5253.

An active pull-down circuit is built into the devices to clamp the output voltage when it rises beyond normal regulation, discharging it automatically by connecting the output to ground through a 100-Ω n-channel MOSFET when the device is put in shutdown mode. This provides better transient response and regulation. Reverse battery protection limits the reverse current flow to approximately 1 µA to prevent damage to the IC in the event that a reversed battery is applied at the input. Short circuit and thermal protection are also built in.

The SiP21101 provides an extremely quiet voltage source because of an external noise bypass capacitor connected to its BP pin that reduces noise to only 30 µV(rms), a significant benefit for RF applications. The same pin on the SiP21102, which has a noise output of 75 µV(rms), functions as an error flag output that goes low when the VOUT drops 4% below its normal voltage.

The SiP21101 and SiP21102 use ceramic capacitors or tantalum capacitors, giving designers a flexible choice of magnetic components.

Samples and production quantities are available now for most voltage options, with lead times of 6 to 8 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###
 
LDO Regulator
 

Products mentioned:

 

This release in:

About Vishay
Brands
Careers
Contacts
Ethics
Investor Relations
Product News
2008 releases
2007 releases
2006 releases
2005 releases
2004 releases
*2003 releases
*2002 releases
*2001 releases
*2000 releases
*1999 releases
Trade Shows
Vishay History
Products A-Z
Company Info:   Press ·  Investors ·  Contacts ·  More...
Privacy & Legal · Your Account