Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

Vishay's New Zero Crossing 1.5-kV/μs dV/dt Phototriacs Provide Off-Line Control of AC Voltages


Optocouplers

Products mentioned:

VO3062/3063
VO3062/3063
For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

This release in:

MALVERN, Pennsylvania — September 28, 2005 μ Vishay Intertechnology, Inc. (NYSE: VSH) today announced the VO3062 and VO3063, two new zero crossing 1.5-kV/μs dV/dt phototriacs designed to isolate low-voltage logic from ac voltages up to 380 V.

The phototriacs consist of a GaAs infrared LED that is optically coupled to a monolithic photosensitive zero crossing triac detector chip. A low-input trigger current facilitates an easy interface with microcontrollers and digital logic. The VO3063 requires a maximum trigger current of 5 mA to latch output, while the VO3062 requires a maximum trigger current of 10 mA. The devices are available in 6-pin DIP, 400-mil DIP, and SMD packages.

Rated with a 600-V blocking voltage, the phototriacs can provide isolation between dc and ac voltages on 120-V, 240-V, and 380-V ac lines, giving designers a 2X or better safety factor for control of off-line voltages up to 240 V.

The VO3062 and VO3063 are designed for control of resistive, inductive, or capacitive loads including motors, solenoids, high-current thyristors, and relays. Optimized for noisy environments, typical applications for the new devices will include refrigerators, air conditioners (HVAC), dishwashers, vending machines, industrial controls, ac motor drives, switches, switching power supplies, and solenoid/valve controls.

The VO3062 and VO3063, in which the new “VO" part number prefix indicates “Vishay optocoupler," are direct replacements for industry-standard 1.0-kV/μs dV/dt phototriacs.

Samples and production quantities of the new phototriacs are available now, with lead times of six to eight weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###
Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword