Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

Vishay's New 0.1-W Surface-Mount Power Metal Strip® Resistor Delivers Industry-Low 15-mΩ Resistance for Compact 0603 Package Size


power metal strip

Products mentioned:

WSL0603
For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

This release in:

MALVERN, PENNSYLVANIA — October 19, 2005 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced a new 1/10-W surface-mount Power Metal Strip® resistor that is the industry's smallest such device to combine a low 15-mΩ to 100-mΩ resistance value range, a tight tolerance of 1%, and low RTC values down to ±75 ppm/°C.

Available in the compact 0603 package size, the new Vishay Dale WSL0603 resistor serves in all types of current-sensing, voltage division, and pulse applications. It is intended for power management in cell phones and pagers; electronic automotive systems including engine controls, audio electronics, and climate controls; and disc drive motor control and dc to dc converters in computers.

With its very small footprint, low resistance values, and low RTC, the new resistor facilitates current-sensing accuracy, which in turn allows designers to use lower-cost ICs. The surface-mount WSL0603 resistor may be used in lieu of larger components or multiple high-value resistors running in parallel to provide space savings on the printed circuit board, thereby enabling design of smaller and lighter end products.

In addition to a power rating of 0.1 W, the Vishay Dale WSL0603 offers low inductance values from 0.5 nH to 5 nH, excellent frequency response, and low thermal EMF. It is rated for an operating temperature range of –65 °C to +170 °C.

The new device, which features an all-welded construction with solderable terminations, is easily placed with automated assembly equipment. It is available with a solid metal nickel-chrome alloy resistive element.

The WSL0603 is available in tape-and-reel packaging. Samples and production quantities of the new resistor are available now, with a lead time of four to five weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Power Metal Strip is a registered trademark of Vishay Intertechnology, Inc.

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword