Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

Vishay TR3 Molded Tantalum Chip Capacitors Offer ESR Values Down to 0.035 Ω and Ripple-Current Handling Up to 2.07 A

New TANTAMOUNT ® Capacitors Are Suited for Broad Range of End Systems


TR3 Molded Tantalum

Products mentioned:

TR3
For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

This release in:

MALVERN, PENNSYLVANIA — November 11, 2005 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced the release of new TR3 series molded tantalum chip capacitors that provide high efficiency with ESR values down to 0.035 Ω and maximum ripple current values up to 2.07 A (100 kHz, 470 μF).

Low ESR values allow for more efficient filtering in dc-to-dc conversion applications, while the devices' ability to handle high currents is key in microprocessor bulk energy storage applications. The new Vishay Sprague TR3 capacitors are intended for applications in telecom, automotive, computer, industrial, commercial, medical, and avionics end systems.

In addition to providing very low ESR values and a high ripple current handling capability, the new tantalum capacitors feature a proven solid tantalum construction that ensures long-term reliability. Outstanding stability over time and temperature further enhances the TR3 devices' performance and reliability.

TR3 devices are available in five molded case sizes — A, B, C, D, and E — with 100 percent tin terminations (RoHS-compliant), or 90/10 Sn/Pb terminations upon request. Devices in the B, C, D, and E case sizes are 100 percent surge-current-tested. All TR3 capacitors meet EIA 535BAAE and IEC QC300801/US0001 specifications. The capacitors' compatibility with high-volume pick-and-place equipment simplifies assembly.

Capacitance values for TR3 tantalum chip capacitors range from 0.47 μF to 680 μF with standard capacitance tolerances of ±10% and ±20%. Voltage ratings range from 4 WVDC to 50 WVDC. The operating temperature range for the new devices is -55 °C to +85 °C, or +125 °C with voltage derating.

Samples and production quantities of the new TR3 molded tantalum chip capacitors are available now, with lead times of four to six weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

TANTAMOUNT is a registered trademark of Vishay Intertechnology, Inc.

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword