VishayOne of the world's largest manufacturers of discrete semiconductors and passive components
Vishay ProductsVishay ProductsCompany InfoCompany InfoCompany Info
Company Info:Press Room:2005 Releases:Updated Technical Guide to Bulk MetalĀ® Foil Resistors
For more information:
Media contact: e-mail andrew.post@vishay.com
Sales contact: http://www.vishay.com/resistors-discrete/metal-foil/
 

Vishay Releases Updated Technical Guide to Bulk Metal® Foil Resistors

Malvern, Pa. — November 16, 2005 — Vishay Intertechnology, Inc. (NYSE: VSH) announces that it has released an updated version of its capabilities brochure on ultra-high-precision Bulk Metal® foil resistors. The brochure, titled Seven Technical Reasons to Specify Bulk Metal® Foil, highlights the features and benefits of these resistors, which outperform all other types of resistors available. Bulk Metal Foil is used primarily in demanding analog applications. The updated brochure includes a new specification for power coefficients of resistance. It also describes a new alloy (Z- Foil®) that improves the existing low temperature coefficient of resistance to almost zero.

Invented by Dr. Felix Zandman in 1962, Bulk Metal foil resistors were (together with foil resistance strain gages), the first products manufactured and marketed by Vishay. Over the years, as Vishay has grown from the start-up company founded by Dr. Zandman to become one of the world's largest manufacturers of discrete semiconductors and passive electronic components, Dr. Zandman — now Chairman of the Board, Chief Technical Officer, and Chief Business Development Officer — has spearheaded an ongoing series of improvements to the original Bulk Metal foil resistor product line. These improvements include Z-Foil, which provides an absolute temperature coefficient of resistance (TCR) of 0.2 ppm/°C.

Seven Technical Reasons to Specify Bulk Metal® Foil is designed to help educate new circuit design engineers and others who need to use resistors for applications that require precision, stability, and reliability. As explained in the brochure, Bulk Metal foil resistors feature a TCR that is lower than that of all other types of resistors. The lower the TCR, the better a resistor can maintain its precise value despite ambient temperature variations and self-heating when power is applied.

The brochure provides a thorough overview of the areas in which Bulk Metal foil technology outperforms other resistor technologies:
   1. Stability of resistance value when a resistor's temperature changes.
      •Low temperature coefficient of resistance (TCR). Resistance change due to changes in ambient temperature: to 0.2 ppm/°C.
      •Low power coefficient of resistance (PCR). Resistance change due to self-heating when power is applied: 5 ppm at rated power. (Precision current-sensing applications)
   2. Resistance tolerance to 0.001%.
   3. Load-life stability to 0.005% at +70 °C for 2000 hours.
   4. Current noise of < -40 dB.
   5. Response time to 1 nanosecond without ringing.
   6. Low thermal EMF: < 0.05 µV/°C.
   7. Non-measurable voltage coefficient.
   8. Rise time of 1 nanosecond.

Seven Technical Reasons to Specify Bulk Metal® Foil is available on the Vishay Web site at http://www.vishay.com/resistors-discrete/metal-foil/related

To obtain printed copies of Seven Technical Reasons to Specify Bulk Metal® Foil, please contact the appropriate Vishay literature distribution center listed below. Please include order number VSA-PL0007-0509 with your request.

The Americas
Fax: +1-402-563-6569

Europe and Israel
Fax: +49 71 31 67 2423

Asia
Fax: +49 71 31 67 2423

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

 
 
About Vishay
Brands
Careers
Contacts
Ethics
Investor Relations
Product News
2008 releases
2007 releases
2006 releases
2005 releases
2004 releases
*2003 releases
*2002 releases
*2001 releases
*2000 releases
*1999 releases
Trade Shows
Vishay History
Products A-Z
Company Info:   Press ·  Investors ·  Contacts ·  More...
Privacy & Legal · Your Account