Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

New Vishay Siliconix Synchronous Buck Step-Down Controller ICs Handle 10-A Currents, Provide Industry-Low Outputs to 0.6 V With 93% Efficiency


 Step-Down Controller ICs

Products mentioned:

SiP12201
SiP12202
For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

This release in:

MALVERN, Pa. — November 28, 2005 — Vishay Intertechnology, Inc. (NYSE: VSH), today released two new synchronous buck step-down controller ICs designed to operate with external MOSFETs — and a minimum of external components — in dc to dc converter circuits that require output currents upwards of 10 A.

The high-voltage SiP12201 and low-voltage SiP12202 controllers both are designed to enable flexible, efficient voltage conversion in a broad range of applications in battery-powered, telecom, and industrial end systems. The new devices’ synchronous buck architecture allows voltages to be converted with efficiencies of 93%, prolonging battery life while lowering heat in enclosed field-mounted or rack-mounted systems and reducing the need for cooling systems.

Input voltage range is 4.2 V to 26 V for the SiP12201 and 2.7 to 5.5 V for the SiP12202. Adjustable output voltages for the two devices range from 0.6 V to 20 V for the SiP12201 and from 0.6 V to 5.5 V for the SiP12202. The ability to reach 0.6 V at the low end is a unique capability for a device with a 500-kHz operating frequency and ensures the SiP12201 and SiP12202 will be able to satisfy the future requirements of lower voltages, predicted to decrease to 0.6 V during the next decade.

SiP12201 High-Voltage Step-Down Controller

The high-voltage SiP12201 synchronous buck step-down controller is designed for industrial control; wireless and cable modems; set-top boxes; LCD TVs; telecom power supplies and servers; point of load (POL) modules; and for delivering regulated power to microprocessors, ASICs, FPGAs, and DSPs in a wide variety of end products. Able to drive n-channel MOSFETs for both the high-side and low-side in a synchronous converter, the SiP12201 helps to reduce overall design costs by allowing the use of two lower-cost n-channel devices instead of one n-channel and one p-channel device. The SiP12201 also offers the advantage of 500 kHz operation, which allows the use of smaller passive components in converter designs.

SiP12202 Low-Voltage Step-Down Controller

The low-voltage SiP12202 synchronous buck step-down controller is intended for power conversion in battery-powered electronics, as well as in notebook and desktop computers and a wide range of other systems using point-of-load or distributed power converters. The controller can be set to 100% duty cycle to assure continued efficiency during low input-voltage conditions. In the event of a low-battery condition, the chip is able to operate as a low dropout (LDO) regulator by going to 100% duty cycle.

The SiP12202 drives an n-channel MOSFET on the low side and a p-channel MOSFET on the high side. Use of the p-channel MOSFET on the high side eliminates the need for an external charge pump while also simplifying the high-side gate driver. High-frequency operation up to 500 kHz enables use of smaller passive components for more compact end systems.

New SiP12201 and SiP12202 Step-Down Controller ICs: Summary Table

Device Input Voltage (V) Adjustable Output (V) Converter Load max. (A) Frequency max. (kHz) External MOSFETs
SiP12201 4.2 to 26 0.6 to 20 10 500 Drives n-channel MOSFET for high-side and low-side
SiP12202 2.7 to 5.5 0.6 to 5.0 10 500 Drives p-channel MOSFETs high-side and n-channel MOSFETs low-side

Because Vishay provides compatible controller and MOSFET devices, designers have access to the best complete solutions for high- and low-voltage step-down applications. The SiP12201 is optimized for use with Vishay’s Si7114DN n-channel power MOSFETs, while the SiP12202 is optimized for use with the p-channel Si7106DN p-channel and Si7110DN n-channel power MOSFETs.

Both of the new step-down controllers include a combination compensation/shutdown pin, as well as additional protection features such as undervoltage lockout, power good output, output-current limit, and thermal shutdown. Internal soft start prevents voltage spikes during start up. Each controller is available in a lead (Pb)-free MLP33-10 package and is specified to operate over the range of -40 °C to +85 °C.

Samples and production quantities of the new synchronous buck step-down controller ICs are available now, with lead times of six to seven weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword