Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

Vishay RFWaves Reference Design for USB-Based Wireless Headset Features 2.4-GHz Wireless Link, 16-Bit PCM Audio Quality, Range Up to 25 Meters


For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

This release in:

MALVERN, PENNSYLVANIA — November 30, 2005 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced the release of a complete Vishay RFWaves reference design for a USB-based wireless headset using a fully digital 2.4-GHz wireless link. Target applications for the system include VoIP, PC-based cordless telephony, and PC-based “intelligent” toys.

The new design uses the Vishay RFWaves RFW322-M 3-Mbps direct sequence spread spectrum (DSSS) half duplex transceiver as its core component, and includes specifications for both the wireless headset/handset and the USB dongle.

The RFW322-M provides an output power of 7 dBm and receiver sensitivity of -75 dBm while delivering 16-bit PCM, 8000 samples/second voice quality. The specified operating range for the design is 6 meters and can be extended to 25 meters with the addition of an RF power amplifier. The high 2.4-GHz bandwidth of the RFW322-M and the exceptional link robustness results in a very reliable and high-quality voice link. The use of printed diversity antennas for the USB further helps to overcome link losses.

The USB dongle component of the reference design specifies the use of a microcontroller to exchange voice/data packets with the PC, to execute a proprietary wireless communication protocol to transfer data over the air, and to perform an antenna diversity algorithm. The dongle uses the Vishay RFWaves RFW322-M as its wireless transceiver. The dongle is powered by the USB port and typically draws 70 mA.

In the remote headset/handset unit, a microcontroller executes the proprietary communication protocol to exchange data with the USB dongle, while feeding incoming data to a high-quality mixed-signal codec. The codec provides analog signals for the speaker and microphone in the headset or handset. The remote unit draws 40 mA and is designed to run for up to four hours from a single lithium ion battery cell.

The system has been designed and tested to coexist with 802.11b/g and Bluetooth® and is compliant with FCC, ETSI, and Telec regulations.

Complete details of the reference design are available on request from shiriz@rfwaves.com.

Documents on transceiver module and reference design:
Datasheet on RFW-322-M transceiver module
Datasheet on RFW-322-M-PA transceiver module with power amplifier
Product overview on WHS322 VoIP wireless headset reference design

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword