Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

Vishay's New CDHV Thick Film Chip Resistor Dividers Deliver <0.03 % Ratio Stability With Voltages Up to 3 kV


CDHV Thick Film Chip Resistor Dividers

Products mentioned:

CDHV
For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

This release in:

MALVERN, Pa. — January 13, 2006 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced the CDHV, a surface-mount chip resistor divider with a small size profile that achieves outstanding ratio stability under high voltages. The new resistor divider is designed for use in high-voltage power supplies, power switching equipment, and inverter controls.

Manufactured with an alumina substrate, the CDHV is capable of handling voltages up to 3 kV, with a voltage coefficient down to 5 ppm/V. It provides resistance values of 1 megohm to 20 gigohms that are available in a broad range of standard and custom resistance ratios from 10:1 to 500:1, with outstanding ratio stability of <0.03 % at full power and 70 °C at 2,000 hours. Absolute resistance tolerance options range from ±20 % down to ±1 %, with ratio tolerance options to 1 %. Its temperature coefficient of resistance is available to ±100 ppm/°C over a –55 °C to +150 °C operating range.

The CDHV is housed in a small 2512 case and has a choice of top-only and wraparound terminations. Dimensions of the top-only resistor divider are 0.240 in. by 0.126 in. [6.10 mm by 3.20 mm] with a profile of 0.025 in. [0.635 mm]. The wraparound version has a slightly increased length of 0.250 in. [6.35 mm]. Both versions are available in tape-and-reel packaging.

Samples and production quantities of the new CDHV resistor divider are available now, with lead times of six to eight weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword