Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

New Vishay Siliconix Boost Converter ICs Provide 85 % Efficiency at 500 mA Down to 1 mA From Battery Voltages as Low as 0.85 V


ICs

Products mentioned:

SiP12502
SiP12503
For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

This release in:

MALVERN, Pa. — February 22, 2006 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced the release of two new boost converter ICs designed to maximize the power available from single- or dual-cell NiMH or alkaline battery packs by providing 85 % dc-to-dc conversion efficiency and operating from battery voltages as low as 0.85 V.

Delivering this high level of efficiency over a broad current range of 1 mA to 500 mA, the new ICs will prolong operating time and reduce component count in portable and battery-powered electronics such as cordless phones, wireless handsets, PDAs, two-way pagers, digital cameras, GPS receivers, MP3 players, and medical diagnostic tools, as well as in LCD and OLED bias systems and wireless LANs and routers.

The new devices offer a choice of fixed 2-V, 3.3-V, and 5-V (SiP12502) or adjustable 2-V to 5-V (SiP12503) output voltages with an 0.85-V to 5-V input voltage range. An internal low-resistance power MOSFET switch enables start-up at the low 0.85-V input voltage, and thus maximizes the useful power available from battery cells. The integrated MOSFET is rated for a low 0.24 Ω impedance at a 3.3 V output. An antiringing control switch minimizes EMI and simplifies circuit layout, reducing design time.

The ability to automatically switch between PWM operation under normal load conditions and PFM mode under light load conditions maximizes efficiency. A low shutdown current of <1 μA further helps to prolong battery life, while overvoltage and thermal shutdown protection help to ensure reliable operation. The converters are powered from the output voltage supply. Integrated features include UVLO and soft start, which addresses inrush current concerns. The fixed-output SiP12502 provides a power-good output on pin 4.

The devices' voltage-mode control loop is internally compensated to further simplify converter design and reduce external parts count. Each device requires only four external components — an inductor, a diode, and two capacitors ― for a complete step-up converter.

Both boost converter ICs are available in a lead (Pb)-free, 6-pin, thermally enhanced PowerPAK® MLP33 (DFN-6, 3x3) package and are specified for an industrial temperature range of -40 °C to +85 °C.

Samples and production quantities of the new SiP12502 and SiP12503 are available now, with lead times of seven to eight weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

PowerPAK is a registered trademark of Siliconix incorporated

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword