VishayOne of the world's largest manufacturers of discrete semiconductors and passive components
Vishay ProductsVishay ProductsCompany InfoCompany InfoCompany Info
Company Info:Press Room:2006 Releases:Vishay's New 60-A, 100-V Dual High-Voltage Trench MOS Barrier Schottky
For more information:
Media contact: e-mail bob.decker@wallstcom.com
Sales contact: http://www.vishay.com/diodes/rectifiers/sales
 

Vishay's New 60-A, 100-V Dual High-Voltage Trench MOS Barrier Schottky (TMBS™) Rectifier Delivers Industry-Low Forward Voltage Drop (Per Leg) of 0.70 V at 30 A and 125 °C

MALVERN, Pa. — May 19, 2006 — Vishay Intertechnology, Inc. (NYSE: VSH) today released a new Trench MOS Barrier Schottky (TMBS) rectifier with the lowest forward voltage ever achieved for this device type.

The new V60100C, rated for 60 A and 100 V in a common-cathode 30 A X 2 configuration, delivers a forward voltage drop (per leg) of 0.70 V at 30 A and 125 °C, and 0.79 V at 30 A and 25 °C.

Optimized for use in 70-W to 800-W high-frequency switchmode power supplies, the low forward voltage drop and superior switching performance of the V60100C reduce power losses and improve the efficiency of the OR-ing diode on the high-voltage output. Typical switchmode power supply applications for the V60100C will include power supplies in servers, industrial computers, and telecom systems. The device will also be used for ac-to-dc rectification in adapters for desktop PCs, servers, notebook PCs, plasma display panel (PDP) TVs, LCD TVs, and monitors.

The V60100C can also be used as an alternative to synchronous rectification (SR) solutions while matching their efficiency and thermal performance.

The V60100C is the latest device in Vishay's TMBS rectifier family, which uses Trench MOS (metal oxide semiconductor) technology to achieve superior performance compared to conventional planar Schottky devices. With their ultra-low forward voltage drops, TMBS rectifiers can perform the same functions with fewer devices, enabling PCB space savings, simplifying designs, and reducing cost for OEMs.

Packaged in the TO-220AB, samples and production quantities of the V60100C are available now, with lead times of 8 to 12 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

 
Trench MOS Barrier Schottky
 

Products mentioned:

 

This release in:

About Vishay
Brands
Careers
Contacts
Ethics
Investor Relations
Product News
2008 releases
2007 releases
2006 releases
2005 releases
2004 releases
*2003 releases
*2002 releases
*2001 releases
*2000 releases
*1999 releases
Trade Shows
Vishay History
Products A-Z
Company Info:   Press ·  Investors ·  Contacts ·  More...
Privacy & Legal · Your Account