![]() |
|
||||||
|
|
|
For more information:
Media contact: e-mail bob.decker@wallstcom.com Sales contact: http://www.vishay.com/power-ics/sales Isolated Synchronous Half-Bridge DC/DC Controller Provides Greater Than 90 % Efficiency At 500 kHz For Step-Down Power ConversionTwo-Chip Solution Saves On Components For Servers and Telecom Power SuppliesMALVERN, Pa. June 21, 2006 Vishay Intertechnology, Inc. (NYSE: VSH) today released a new 500-kHz half-bridge dc-to-dc controller and synchronous rectifier driver that work together as a chipset to enable more efficient 25-W to 300-W telecom and computer power supplies. The new Si9122A half-bridge controller and SiP11203/11204 secondary synchronous rectifier driver offer greater than 90 % dc to dc conversion efficiency even for output voltages below 3.3 V in power supply modules and network cards for fixed telecom systems, central office switching equipment, distributed power systems, intermediate bus converters, and brick converters.
Si9122A Half-Bridge Controller
On-chip control of the dead-time delays between the primary and secondary synchronous signals keeps efficiencies high and prevents shorting of the power transformer. An external resistor sets the switching frequency from 200 kHz to 500 kHz. Advanced monitoring and control circuitry in the Si9122A enables users to set the maximum current in the primary circuit and allows the system to operate a constant current into a short circuit. This same circuitry also provides constant current into large capacitive loads during start-up or when paralleling multiple power supplies. The Si9122A is available in TSSOP-20 or MLP65-20 packages.
SiP11203 and SiP11204 Secondary Synchronous Rectifier Drivers
The SiP11203/11204 and Si9122A interface via a pulse transformer to provide isolated control of the synchronous MOSFETs. The error signal, supplied by the SiP11203/11204, is fed to the Si9122A via an opto-isolator. Together the transformers and the opto-isolator provide isolation between the input and the output. Both ICs are capable of being powered via conventional bias supplies (output inductor winding or power transformer winding), or from the same pulse transformer supplying the gate timing signals, and both parts generate a regulated supply for powering the error amplifier and control circuitry. The two product versions provide a choice of synchronous rectifier turn-off (SiP11203) or turn-on (SiP11204) in the event of an overvoltage condition. During power-up, the SiP11203/11204 ensure that the synchronous rectifiers are held off until the supply voltages are sufficient to guarantee effective operation of the driver circuits. During the soft-start interval, a gradual ramp-up of the synchronous rectifier conduction time is assured. The ICs also allow control of the discharge rate of the synchronous rectifier driver outputs during power-down. Both devices are rated for a 5.5-V to 13-V operating range, feature a regulated internal logic voltage of 5 V, and provide a 2.2-A source and 4 A sink drive capability. They are designed for high-current applications in any topology requiring secondary-side drivers. Each driver is available in a compact MLP44-16 package.
Availability
Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com. ###
| ![]() | ||||
|
|||||
| ||||||