Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

Vishay Broadens Portfolio of Ambient Light Sensors With Surface-Mount 0805 and Leaded 3-mm and 5-mm Devices


For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

This release in:

MALVERN, Pa. — July 7, 2006 — Vishay Intertechnology, Inc. (NYSE: VSH) is adding to its optoelectronics portfolio with three new ambient light sensors that allow automatic control of liquid crystal display (LCD) brightness and enable a number of advanced automotive driver comfort and safety features.

Providing a simple two-pin connection, these sensors will be used to reduce power consumption in consumer electronics applications by controlling keypad backlights and to adjust the brightness of LCDs. In automotive applications, the sensors will enable automatic headlight control, tunnel sensors, and displays that adjust automatically to changes in ambient brightness. As phototransistors, these sensors eliminate the need for an external amplifier.

The three devices launched today give designers a choice of surface-mount 0805 (TEMT6200F) or leaded 5-mm flat-top (TEPT5700) or 3-mm (TEPT4400) packages. The angle of half intensity is ±60° for the TEMT6200F, ±50° for the TEPT5700 and ±30° for the TEPT4400. The TEMT6200F peak wavelength sensitivity is 550 nm, while the TEPT5700 and TEPT4400 are 570 nm, green-yellow on the visible spectrum. These new devices join the previously released TEMT6000 in the surface-mount 1206 package and TEPT5600 in narrow angle 5-mm package to give designers an ambient light sensor portfolio that meets the needs of every application.

In addition to improving display visibility and reducing power consumption, the new devices are an environmentally friendly alternative to cadmium-based photo resistors, the elimination of which has been mandated by Restriction of Hazardous Substances (RoHS) legislation. All three devices are lead (Pb)-free and in accordance with RoHS 2002/95/EC and WEEE 2002/96/EC.

Samples are available now with lead times of 6 weeks.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword