Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

Vishay’s New WSLP1206 1-W Surface-Mount Power Metal Strip® Resistor Is Industry’s First in 1206 Package Size


surface-mount Power Metal Strip resistor
For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

This release in:

MALVERN, PENNSYLVANIA —August 23, 2006 —Vishay Intertechnology, Inc. (NYSE: VSH) today announced a new surface-mount Power Metal Strip® resistor that is the industry’s first 1-W current sensing resistor in the very small 1206 package size. The WSLP1206 resistor features a very low 2-mΩ to 50-mΩ resistance value range, and high-temperature performance up to 170 /°C.

The small size of the WSLP1206 resistor allows it to replace larger current sensing resistors, saving space on the circuit board that in turn will create smaller and lighter products for the consumer. It is intended for current sensing and pulse applications in dc-to-dc converters for computers, VRMs for laptops, and Li-Ion battery safety and management; and electronic automotive systems, including engine controls, multi-media electronics, climate controls, and anti-lock brakes.

Manufactured using proprietary techniques that result in extremely high power and low resistance values, the WSLP1206 features all-welded construction with a solid metal nickel-chrome or manganese-copper alloy resistive element. The resistor offers very low inductance values from 0.5 nH to 5 nH, an excellent frequency response to 50 MHz, and low thermal EMF of less than 3μV/°C.

Samples and production quantities of the new resistor are available now, with a lead time of four to six weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Power Metal Strip is a registered trademark of Vishay Intertechnology, Inc.

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword