VishayOne of the world's largest manufacturers of discrete semiconductors and passive components
Vishay ProductsVishay ProductsCompany InfoCompany InfoCompany Info
Company Info:Press Room:2006 Releases:Vishay's New WSLT2512 1-W, Surface-Mount 2512 Power Metal Strip® Resistor
For more information:
Media contact: e-mail
Sales contact: http://www.vishay.com/resistors-discrete/sales
 

Vishay's New WSLT2512 1-W, Surface-Mount 2512 Power Metal Strip® Resistor Is Industry's First to Offer Temperature Range of –65 °C to +275 °C

MALVERN, PENNSYLVANIA — August 23, 2006 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced a new high-temperature 1-W surface-mount Power Metal Strip® resistor that is the industry's first current sensing resistor in the 2512 case size to operate in a temperature range of –65 °C to +275 °C. The WSLT2512 resistor features a very low 10-mΩ to 500-mΩ resistance value range, a tight tolerance down to ±0.5 %, and low TCR values down to ±75 ppm/°C.

The temperature range of the WSLT2512 allows it to replace larger current sensing resistors with a similar +275 °C maximum operating temperature. Its robust specifications allow the WSLT2512 to be used for current sensing and pulse applications in harsh, high-temperature environments without sacrificing power rating or electrical performance. The range of systems into which the WSLT2512 will be designed includes automotive engine controls, safety controls, multi-media electronics, climate controls, and anti-lock brakes; and industrial oil/gas well drilling, including down hole test/measurement equipment.

Manufactured using proprietary techniques that result in extremely low resistance values, the WSLT2512 features all-welded construction with a solid metal nickel-chrome alloy resistive element. The resistor offers low inductance values, an excellent frequency response to 50 MHz, and low thermal EMF of less than 3 µV/°C.

Samples and production quantities of the new resistor are available now, with a lead time of four to six weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Power Metal Strip is a registered trademark of Vishay Intertechnology, Inc.

 
Surface-Mount 2512 Power Metal Strip®  Resistor
 

Products mentioned:

 

This release in:

About Vishay
Brands
Careers
Contacts
Ethics
Investor Relations
Product News
2008 releases
2007 releases
2006 releases
2005 releases
2004 releases
*2003 releases
*2002 releases
*2001 releases
*2000 releases
*1999 releases
Trade Shows
Vishay History
Products A-Z
Company Info:   Press ·  Investors ·  Contacts ·  More...
Privacy & Legal · Your Account