VishayOne of the world's largest manufacturers of discrete semiconductors and passive components
Vishay ProductsVishay ProductsCompany InfoCompany InfoCompany Info
Company Info:Press Room:2006 Releases:Vishay’s New Z201 Ultra-High-Precision Z-Foil Resistor
For more information:
Media contact: e-mail andrew.post@vishay.com
Sales contact: http://www.vishay.com/resistors-discrete/metal-foil/sales
 

Vishay’s New Z201 Ultra-High-Precision Z-Foil Resistor is First to Combine Very Low Typical TCR of ±0.05 ppm/°C (0 °C to +60 °C), Low PCR of ±5 ppm at Rated Power, Tight Tolerances of ±0.005 % (50 ppm), and Electrostatic Discharge (ESD) Above 25,000 Volts

Improved Device Features Load Life Stability of ±0.005 % and Rise Time of 1 ns Without Ringing

MALVERN, PENNSYLVANIA — December 15, 2006 — Vishay Intertechnology, Inc. (NYSE: VSH) announces the improved Z201 ultra-high-precision Z-Foil resistor, the industry’s first device to provide a very low TCR of ±0.05 ppm/°C from 0 °C to +60 °C and ±0.2 ppm/°C from -55 °C to +125 °C, an excellent PCR (“∆R due to self heating”) of ±5 ppm at rated power, tight tolerances of ±0.005 %, and a load life stability of ±0.005 %.

Vishay’s revolutionary “Z-based” foil technology provides a significant reduction of the resistive component’s sensitivity to ambient temperature variations (TCR) and applied power changes (PCR). This breakthrough level of stability, more than an order of magnitude better than any other resistor technology, allows designers to guarantee a high degree of accuracy in fixed-resistor applications.

Applications for the new Z201 include precision amplifiers; high-precision instrumentation; medical and automatic test equipment; high-end stereo equipment; electron beam scanning and recording equipment; and military, aerospace, and down-hole equipment and instrumentation.

The Z201 device has a load-life stability of ±0.005 % for 2000 hours at 70 °C; a resistance range of 10 Ω to 100 kΩ; a power rating of 0.3 W at 125 °C; current noise < -40 dB; and thermal EMF of 0.1 µV °C max (0.05 typical). It offers high-frequency operation with a rise time of 1.0 ns without ringing, and features a non-inductive, non-capacitive design. The device offers a small package size, and functions as a drop-in replacement for the earlier S102C/K series of resistors.

Despite a great deal of effort during the past decade, electrostatic discharge (ESD) still affects production yields, manufacturing costs, product quality, product reliability, and profitability. Industry experts have estimated actual cost of ESD damage to the electronics industry as running into the billions of dollars annually. The Z201 resistor has an ESD above 25,000 V, putting it well over the top requirements of all three of the highest ESD standard classifications and making it exceptionally insensitive to ESD.

Because of its specifications, the new Z201 will reduce solution costs, allowing designers to rely on consistent resistor performance to overcome the limitations of other components and to reduce the need for end product testing.

Samples and production quantities of the improved Z201 Z-Foil resistor are available now, with lead times of four to six weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

 
Z-Foil Resistors
 

Products mentioned:

 

This release in:

About Vishay
Brands
Careers
Contacts
Ethics
Investor Relations
Product News
2008 releases
2007 releases
2006 releases
2005 releases
2004 releases
*2003 releases
*2002 releases
*2001 releases
*2000 releases
*1999 releases
Trade Shows
Vishay History
Products A-Z
Company Info:   Press ·  Investors ·  Contacts ·  More...
Privacy & Legal · Your Account