Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

Vishay Expands IHLP Family of Low-Profile, High-Current Inductors With New Devices Featuring Maximum Frequency Ranges of 1.0 MHz and 5.0 MHz

New Inductors Offer Low 4.0-mm Profile With Saturation Currents up to 46 A and 90 A, and Inductance Values Down to 0.19 μH


061220ind

Products mentioned:

IHLP-4040DZ-01
IHLP-4040DZ-11
For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

This release in:

MALVERN, Pa. — December 20, 2006 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced the release of the new IHLP-4040DZ-01 and IHLP-4040DZ-11 low-profile, high-current inductors, which feature high maximum frequencies and low inductance values.

The IHLP-4040DZ-11 offers a maximum frequency of 1.0 MHz, while the IHLP-4040DZ-01 features a maximum frequency of 5.0 MHz. Both devices offer inductance values down to 0.19 μH.

Offering very low DCR and the highest inductance for their respective package sizes, the new IHLP inductors serve as high-performing, space- and power-saving solutions for voltage regulator module (VRM) and dc-to-dc converter applications in end products including next-generation mobile devices; notebooks, desktop computers, servers, graphic cards, portable gaming devices, personal navigation systems, personal multimedia devices, and automotive systems; low-profile, high-current power supplies and point of load (POL) converters; distributed power systems; and field-programmable gate arrays (FPGAs).

For applications requiring a frequency range up to 1 MHz, the IHLP-4040DZ-11 offers an inductance range from 0.19 μH up to 100 μH, a saturation current range from 2.25 A up to 46 A, typical DCR from 0.70 mΩ to 249.0 mΩ, and maximum DCR from 0.80 mΩ to 270.0 mΩ. For applications requiring a frequency range up to 5 MHz, the IHLP-4040DZ-01 offers an inductance range from 0.19 μH up to 10 μH, a saturation current range from 12.0 A up to 90 A, typical DCR from 0.875 mΩ to 33.20 mΩ, and maximum DCR from 0.95 mΩ to 36.5 mΩ.

With compact dimensions of 0.405 in. by 0.453 in. [10.3 mm by 11.5 mm] and a very low height profile of 0.158 in. [4.0 mm], the IHLP-4040DZ-01 and IHLP-4040DZ-11 inductors occupy the standard 4040 footprint shared by lower-profile IHLP devices while providing higher rated current and lower DCR values.

The new inductors handle high transient current spikes without hard saturation. Packaged in an RoHS-compliant, 100 % lead (Pb)-free shielded, composite construction that reduces buzz noise to ultra-low levels, the new devices are specified for an operating temperature range of 55 °C to +125 °C with high resistance to thermal shock, moisture, mechanical shock, and vibration.

IHLP-4040DZ-01 and IHLP-4040DZ-11 Table Summary

Device Frequency Range Lo Inductance Saturation Current Typical DCR Max DCR
IHLP-4040DZ-01 <5.0 MHz 0.19 μH - 10 μH 12.0 A - 90 A 0.875 mΩ - 33.20 mΩ 0.95 mΩ - 36.5 mΩ
IHLP-4040DZ-11 <1.0 MHz 0.19 μH - 100 μH 2.25 A - 46 A 0.70 mΩ - 249.0 mΩ 0.80 mΩ - 270.0 mΩ

Samples and production quantities of the new inductors are available now, with lead times of six to eight weeks for large orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###
Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword