Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

Vishay's New Non-Zero-Crossing 1.5-kV/μs dV/dt Phototriac Optocouplers Provide Off-Line Control of AC Voltages up to 380 V


061220opto

Products mentioned:

VO3052
VO3053
For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

This release in:

MALVERN, Pa. — December 20, 2006 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced the VO3052 and VO3053, two new non-zero-crossing 1.5-kV/μs dV/dt phototriac optocouplers designed to isolate low-voltage logic from AC voltages up to 380 V.

The phototriacs consist of a GaAs infrared LED that is optically coupled to a monolithic photosensitive zero-crossing triac detector chip. A low-input trigger current facilitates an easy interface with microcontrollers and digital logic. The VO3053 requires a maximum trigger current of 5 mA to latch output, while the VO3052 requires a maximum trigger current of 10 mA. The devices are offered in the 6-pin DIP package.

Rated with a 600-V blocking voltage, the phototriacs can provide isolation between DC and AC voltages on 120-V and 240-V AC lines, giving designers a 2X or better safety factor for control of off-line voltages up to 240 V.

The VO3052 and VO3053 are designed for control of resistive, inductive, or capacitive loads, including motors, solenoids, high-current thyristors, and relays. Optimized for noisy environments, typical applications for the new devices include refrigerators, air conditioners (HVAC), dishwashers, vending machines, industrial controls, AC motor drives, switches, switching power supplies, and solenoid/valve controls.

The VO3052 and VO3053, in which the new VO part number prefix indicates Vishay optocoupler, are direct replacements for industry-standard 1.0-kV/μs dV/dt phototriacs and companion devices to Vishays zero-crossing VO3062 and VO3063 1.5-kV/μs dV/dt phototriacs.

Samples and production quantities of the new phototriacs are available now, with lead times of six to eight weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###
Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword