Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

Vishay’s New Multi-Channel EMI Filter Arrays Feature Ultra-Compact LLP Leadless Packages For Board Space Savings

Devices Feature Low Profile of 0.6 mm and a Pitch Between Pin to Pin of 0.4 mm


For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

This release in:

MALVERN, PENNSYLVANIA — January 19, 2007 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced the release of three new four-, six-, and eight-channel EMI filters in the ultra-compact LLP leadless packages.

With a low profile of 0.6 mm and a pitch between pin to pin of 0.4 mm, the new VEMI filter arrays are designed to save board space and provide ESD protection in portable electronics for mobile computing, mobile communication, consumer, industrial, automotive, and medical applications.

The new arrays include the four-channel VEMI45AA-HNH, the six-channel VEMI65AA-HCI, and the eight-channel VEMI85AA-HGK. Delivering high-quality filtering, the new devices are capable of attenuating unwanted signals by more than 30 dB over the 900 MHz up to 2.3 GHz frequency range, with a resistance of 100 Ω and an input capacitance of 60pF. Low leakage current helps to prolong battery life.

All three devices provide transient protection for data lines as per IEC 61000 4 2 (ESD) at 30 kV (air and contact discharge) and IEC 61000 4 5 (lightning) from 4 A
(tp = 8/20μs). They also are compliant with RoHS 2002/95/EC and WEEE 2002/96/EC.

New EMI Filter Arrays In Ultra-Compact LLPXX13 Leadless Packages: Summary Table

Part Channel Typical line
resistance
(Ω)
Typical cut-off freq.
(MHz)
Package type
VEMI45AA-HNH 4 100 100 LLP1713
VEMI65AA-HCI 6 100 100 LLP2513
VEMI85AA-HGK 8 100 100 LLP3313

Samples of the new EMI filter arrays in the leadless LLP package are available now. Production quantities will be available in Q1 2007, with lead times of 10 to 12 weeks for large orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###
Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword