Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

Vishay’s New WSLS2512 Surface-Mount Power Metal Strip® Resistor Offers Increased Stability With Low Resistance Change of 0.5 % in Low Resistance Values of 0.01 Ω to 0.1 Ω


070119wsls

Products mentioned:

WSLS2512
For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

This release in:

MALVERN, PENNSYLVANIA — January 19, 2007 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced a new surface-mount Power Metal Strip® resistor that offers improved resistance stability during operation with a maximum resistance change of 0.5 % through a 2000-hour workload. By comparison, the typical current sensing resistor has a resistance stability of ≥1 % through a 1000-hour workload.

The Vishay Dale WSLS2512 devices feature specially selected materials which allow for current sensing in high-temperature (+125 °C), tightened-stability applications that require precision current monitoring of sensitive circuits, such as automotive electronic controls including engine, transmission, and pollution controls.

Manufactured using proprietary techniques that result in extremely low resistance values of 0.01 Ω to 0.1 Ω, the WSLS2512 features all-welded construction with a solid metal nickel-chrome alloy resistive element. The resistor offers low inductance values of 0.5 nH to 2.0 nH, a tight tolerance down to ±0.5 %, and low TCR values down to ±30 ppm/°C.

Samples of the new resistor will be available in February 2007. Production quantities will be available in Q3 2007, with a lead time of eight weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###
Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword