VishayOne of the world's largest manufacturers of discrete semiconductors and passive components
Vishay ProductsVishay ProductsCompany InfoCompany InfoCompany Info
Company Info:Press Room:2007 Releases:Vishay Releases New Sapphire-Based, High-Intensity White SMD LED Series in PLCC-2 Package
For more information:
Media contact: e-mail bob.decker@wallstcom.com
Sales contact: http://www.vishay.com/leds/sales
 

Vishay Releases New Sapphire-Based, High-Intensity White SMD LED Series in PLCC-2 Package

Cost-Effective Devices Offer High Luminous Intensity of 112 mcd to 355 mcd, and 2-kV ESD-Withstand Voltage

MALVERN, PENNSYLVANIA — February 2, 2007 — To meet the increasing demand for white SMD LEDs, Vishay Intertechnology, Inc. (NYSE: VSH) today released a new series of sapphire-based, high-intensity white SMD LEDs that offer highly efficient InGaN technology at a very low price.

The new VLMW41xx series of SMD LEDs provides cost-effective illumination for applications including backlighting in automotive dashboards and switches; indicators and backlighting in telecommunications systems, audio and video equipment, and office equipment; and flat backlighting for LCDs, switches, and symbols in general use.

The devices offer a 60° angle of half-intensity, an extremely high luminous intensity ranging from 112 mcd to 355 mcd, and a typical color temperature of 5500 K. The LEDs feature an ESD-withstand voltage up to 2 kV, in accordance with JESD22-A114-B.

The package for the new series is the EIA- and ICE-standard PLCC-2, which consists of a lead frame embedded in a white thermoplast. The reflector inside the package is filled with a mixture of epoxy and TAG phosphor. The TAG phosphor converts the blue emission partially to yellow, which mixes with the remaining blue to produce white.

Preconditioned according to JEDEC Level 2a standards, the PLCC-2 package is lead (Pb)-free and RoHS-compliant. CECC compatibility with infrared, vapor phase, and wave solder processes ― as well as automatic placement equipment and IR reflow soldering ― simplifies handling and automatic assembly. The VLMW41xx devices are qualified according to AEC Q101.

Available in 8 mm tape, samples and production quantities of the VLMW41xx high-intensity SMD LEDs are available now, with lead times of five weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###
 
070202smdled
 

Products mentioned:

 

This release in:

About Vishay
Brands
Careers
Contacts
Ethics
Investor Relations
Product News
2008 releases
2007 releases
2006 releases
2005 releases
2004 releases
*2003 releases
*2002 releases
*2001 releases
*2000 releases
*1999 releases
Trade Shows
Vishay History
Products A-Z
Company Info:   Press ·  Investors ·  Contacts ·  More...
Privacy & Legal · Your Account