|
For more information: Four New IHLP Low-Profile, High-Current Inductors Feature Low Profiles of 1.2 mm and 2.0 mm With Maximum Frequency Ranges of 1.0 MHz and 5.0 MHzNew Inductors Offer Inductance Values From 0.047 μH to 4.7 μH
MALVERN, PENNSYLVANIA — February 9, 2007 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced the release of four new low-profile, high-current inductors that feature high maximum frequencies and low inductance values. The IHLP-1616AB-11 and IHLP-1616BZ-11 inductors offer a maximum frequency of 1.0 MHz, while the IHLP-1616AB-01 and IHLP-1616BZ-01 feature a maximum frequency of 5.0 MHz. The inductance range for this new series is from 0.047 μH to 4.7μH. Offering the lowest DCR/μH for their respective package sizes, the new IHLP inductors serve as high-performing, space- and power-saving solutions for voltage regulator module (VRM) and dc-to-dc applications such as point-of-load converters, distributed power systems, and voltage regulation for FPGAs. Target end products for the devices include next-generation mobile devices; notebooks, desktop computers, servers, graphic cards, portable gaming devices, personal navigation systems, personal multimedia devices, and automotive navigation and multimedia entertainment systems. Other applications include medium- to high- current noise filtering and dc-to-dc boost converters for white LED driver circuits. New Low-Profile, High-Current inductors: Summary Table
All four devices released today feature compact dimensions of 0.160 in. by 0.175 in. [4.06 mm by 4.45 mm], and occupy the new 1616 footprint. The IHLP-1616AB-01 and IHLP-1616AB-11 inductors offer very low height profiles of 0.047 in. [1.2 mm], and the IHLP-1616BZ-01 and IHLP-1616BZ-11 inductors offer low profiles of 0.079 in. [2.0 mm]. The new inductors handle high transient current spikes without hard saturation. Their shielded, composite construction is RoHS-compliant and 100 % lead (Pb)-free. The new devices are specified for an operating temperature range of 55 °C to +125 °C with high resistance to thermal shock, moisture, mechanical shock, and vibration. Samples and production quantities of the new inductors are available now, with lead times of six to eight weeks for large orders.
Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com. |