Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

Vishay Releases New Wide-Band IR Sensor for Code Learning and IR Extender Applications

New Sensor Covers Bandwidth of 30 kHz to 455 kHz With Supply Voltages From 2.7 V to 5.5 V


070209wbir

Products mentioned:

TSOP98200
For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

This release in:

MALVERN, Pa. — February 9, 2007 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced the release of a new and unique device implementing a wide-band IR sensor for code learning and IR extender applications.

The TSOP98200 has been developed to address the growing need for an AC-coupled IR sensor covering the entire remote control bandwidth of 30 kHz to 455 kHz. The new device features a photo diode and a wide-band amplifier mounted within a 3-pin epoxy- encapsulated module with an integrated semi-cylindrical lens.

In contrast to many available IR sensors, the new device is AC coupled to prevent activating the sensor from constant light sources such as tungsten bulbs or sunlight. This feature provides optimal reception of the IR code even in the presence of these light sources.

The new IR sensor is specified for operation with supply voltages from 2.7 V to 5.5 V, while the TTL- and CMOS-compatible output can be directly connected to digital circuitry such as a microprocessor. The small package simplifies the design and layout of compact IR extender and code learning systems.

Samples and production quantities of the new TSOP98200 IR sensors are available now, with lead times of 10 weeks for large orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###
Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword