![]() |
|
||||||
|
|
|
For more information:
Media contact: e-mail bob.decker@wallstcom.com Sales contact: http://www.vishay.com/ir-receiver-modules/sales Vishay Releases New Wide-Band IR Sensor for Code Learning and IR Extender ApplicationsNew Sensor Covers Bandwidth of 30 kHz to 455 kHz With Supply Voltages From 2.7 V to 5.5 VMALVERN, Pa. February 9, 2007 Vishay Intertechnology, Inc. (NYSE: VSH) today announced the release of a new and unique device implementing a wide-band IR sensor for code learning and IR extender applications. The TSOP98200 has been developed to address the growing need for an AC-coupled IR sensor covering the entire remote control bandwidth of 30 kHz to 455 kHz. The new device features a photo diode and a wide-band amplifier mounted within a 3-pin epoxy- encapsulated module with an integrated semi-cylindrical lens. In contrast to many available IR sensors, the new device is AC coupled to prevent activating the sensor from constant light sources such as tungsten bulbs or sunlight. This feature provides optimal reception of the IR code even in the presence of these light sources. The new IR sensor is specified for operation with supply voltages from 2.7 V to 5.5 V, while the TTL- and CMOS-compatible output can be directly connected to digital circuitry such as a microprocessor. The small package simplifies the design and layout of compact IR extender and code learning systems. Samples and production quantities of the new TSOP98200 IR sensors are available now, with lead times of 10 weeks for large orders. Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com. ###
| ![]() | ||||
|
|||||
| ||||||