VishayOne of the world's largest manufacturers of discrete semiconductors and passive components
Vishay ProductsVishay ProductsCompany InfoCompany InfoCompany Info
Company Info:Press Room:2007 Releases:Vishay’s New VJ HVArc Guard™ Surface-Mount C0G MLCCs
For more information:
Media contact: e-mail andrew.post@vishay.com
Sales contact: http://www.vishay.com/capacitors/ceramic-multilayer/sales
 

Vishay’s New VJ HVArc Guard™ Surface-Mount C0G MLCCs are Industry’s First Designed to Prevent Surface Arc-Over at High Voltages With Capacitance Ranges of 10 pF to 2700 pF

Devices Offer Twice the Voltage Breakdown of Standard Capacitors, Feature Voltage Ratings From 1000 VDC to 1500 VDC

MALVERN, PENNSYLVANIA— February 14, 2007— Vishay Intertechnology, Inc. (NYSE: VSH) today announced the release of the industry’s first surface-mount C0G multilayer ceramic chip capacitors (MLCCs) designed to prevent surface arc-over. The new devices provide maximum capacitance in high-voltage ratings and an increased capacitor voltage breakdown.

The new VJ0805, VJ1206, and VJ1210 HVArc Guard MLCCs feature a unique and patent-pending internal design structure that prevents surface arc-over at high voltages. This design allows for higher capacitances and facilitates the use of smaller case sizes in high-voltage products, allowing for device miniaturization and reducing component cost.

Optimized for applications including buck and boost dc-to-dc converters, voltage multipliers for flyback converters, and lighting ballast circuits, the new devices will be used in lighting systems and power supplies for medical, computer, motor control, and telecommunications applications.

The three HVArc Guard capacitors released today feature capacitances ranging from 10 pF to 2700 pF in smaller case sizes than standard high-voltage MLCCs, and offer twice the standard voltage breakdown with voltage ratings from 1000 VDC to 1500 VDC. The devices eliminate the need for conformal coating, and can replace wire leaded through-hole capacitors.

Samples and production quantities of the new VJ HVArc Guard surface-mount C0G MLCCs are currently available, with lead times of approximately eight weeks.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###
 
070214mlcc
 

Products mentioned:

 

This release in:

About Vishay
Brands
Careers
Contacts
Ethics
Investor Relations
Product News
2008 releases
2007 releases
2006 releases
2005 releases
2004 releases
*2003 releases
*2002 releases
*2001 releases
*2000 releases
*1999 releases
Trade Shows
Vishay History
Products A-Z
Company Info:   Press ·  Investors ·  Contacts ·  More...
Privacy & Legal · Your Account