VishayOne of the world's largest manufacturers of discrete semiconductors and passive components
Vishay ProductsVishay ProductsCompany InfoCompany InfoCompany Info
Company Info:Press Room:2007 Releases:Vishay’s New 75-V, 2-A Half-Bridge MOSFET Driver Targets Automotive, Power Conversion, and Class D Audio Applications
For more information:
Media contact: e-mail bob.decker@wallstcom.com
Sales contact: http://www.vishay.com/power-ics/sales
 

Vishay’s New 75-V, 2-A Half-Bridge MOSFET Driver Targets Automotive, Power Conversion, and Class D Audio Applications

SiP41111 Features 9-V to 13.2-V Supply Voltage Range

MALVERN, Pa. — February 26, 2007 — Vishay Intertechnology, Inc. (NYSE: VSH), today announced the release of a high-frequency 75-V half-bridge n-channel MOSFET driver IC that delivers a 2-A peak sink and source gate driver current.

The new SiP41111 is particularly well suited for automotive applications, which often require voltages up to 40 V or 60 V. The 75 V MOSFET driver may be used in high-intensity discharge lamps in automobiles, as well as in high-voltage buck converters, push-pull converters, full- and half-bridge converters, active clamp forward converters, power supplies, motor control, and class D audio systems in a variety of end products.

The SiP41111 features a maximum bootstrap supply voltage up to 75-V, accommodates a broad supply voltage range from 9 V to 13.2 V, and is capable of driving a 1,000-pF load with typical rise and fall times of 10 ns. Typical delay match and high-low match times of 6.5 ns enable the fast propagation times required for multi-megahertz circuits. An on-chip 1.5-Ω bootstrap diode helps to reduce external component count. Undervoltage protection pushes the outputs to low in the event of an undervoltage event, after which the device turns on again automatically.

The SiP41111 is pin-compatible with the HIP2100 and HIP2101. Offered in the SOIC-8 and thermally enhanced PowerPAK® SOIC packages, samples and production quantities of the SiP41111 are available now, with lead times of 8 to 10 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

PowerPAK is a registered trademark of Siliconix incorporated.

 
070226mosfet
 

Products mentioned:

 

This release in:

About Vishay
Brands
Careers
Contacts
Ethics
Investor Relations
Product News
2008 releases
2007 releases
2006 releases
2005 releases
2004 releases
*2003 releases
*2002 releases
*2001 releases
*2000 releases
*1999 releases
Trade Shows
Vishay History
Products A-Z
Company Info:   Press ·  Investors ·  Contacts ·  More...
Privacy & Legal · Your Account