VishayOne of the world's largest manufacturers of discrete semiconductors and passive components
Vishay ProductsVishay ProductsCompany InfoCompany InfoCompany Info
Company Info:Press Room:2007 Releases:Vishay Releases New Schottky Rectifiers
For more information:
Media contact: e-mail bob.decker@wallstcom.com
Sales contact: http://www.vishay.com/diodes/rectifiers/sales
 

Vishay Releases New Schottky Rectifiers Rated to 1 A and Transient Voltage Suppressors Rated to 100 W in Miniature MicroSMP™ Power Package With Space-Saving 2.5-mm by 1.3-mm Footprint

Junction-To-Lead Thermal Resistance is 30°C/W For Schottky Diodes and 20°C/W for TVS

MALVERN, PENNSYLVANIA — April 18, 2007 — Vishay Intertechnology, Inc. (NYSE: VSH) today launched a new MicroSMP™ miniature package type for Schottky rectifiers and transient voltage suppressors (TVS) that provides high current power density and low thermal resistance for space savings and improved reliability.

With a low 0.65-mm height and 2.5-mm by 1.3-mm footprint, the new Schottky MicroSMP rectifiers are designed to provide secondary rectification and freewheeling diode functions for miniature ac-to-dc and dc-to-dc converters; flywheel and polarity protection for miniature power converters and portable electronic equipment such as digital cameras, MP3 players, navigation systems, GPS, and cellular phones; and polarity protection of power lines and signal lines for automotive and industrial systems.

The new MicroSMP TVS devices are optimized for power and signal line protection for microprocessors, signal processing ICs, and logic circuits; and high-power voltage regulation for non-sensitive input voltage circuits in automotive and industrial electronics. These new devices improve on all previous TVS products in similar package types by combining ESD transient protection with a superior surge clamping capability.

Featuring a low forward voltage drop, the six new Schottky rectifiers released today are rated up to 1 A at a 110 °C lead temperature, while the two new voltage suppressors feature a peak pulse current of 100 W at a 10/1000-µs waveform. All the devices offer a high 25-A forward surge current capability for an 8.3-ms pulse. Low junction-to-lead thermal resistance of 30 °C/W for the Schottky rectifiers and 20 °C/W for the TVS devices provides improved reliability and a longer operational life span.

The devices’ single-chip, surface-mount MicroSMP package features solder pads that are compatible with other SMD devices, so no modification is needed to the PCB layout when they are used as higher-performing upgrades to existing devices.

Rectifier Specification Table

Vishay P/N IF
(A)
VRRM
(V)
VF at IF and TJ IFSM
(A)
TJ max
(°C)
VF
(V)
IF
(A)
TJ
(°C)
MSS1P2L 1 20 0.40 1 125 25 150
MSS1P3L 1 30 0.40 1 125 25
MSS1P3 1 30 0.46 1 125 25
MSS1P4 1 40 0.46 1 125 25
MSS1P5 1 50 0.60 1 125 25
MSS1P6 1 60 0.60 1 125 25

TVS Specification Table

P/N Stand-off
Voltage
Breakdown
Voltage
At 10/1000µS 8/20µS Pd
(W)
TJ max
(°C)
VWM
(V)
VBR(V) PPPM(W) VC IPPM(A) VC IPPM(A)
MSP3V3 3.3 4.1 at
1 mA
100 7.3 13.7 11.0 75 1 150
MSP5.0A 5.0 6.7 at
10 mA
100 9.2 10.9 -- -- 1 150

Samples and production quantities of the new Schottky and TVS devices in the MicroSMP package are available now with lead times of eight weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###
 
070418urg
 

This release in:

About Vishay
Brands
Careers
Contacts
Ethics
Investor Relations
Product News
2008 releases
2007 releases
2006 releases
2005 releases
2004 releases
*2003 releases
*2002 releases
*2001 releases
*2000 releases
*1999 releases
Trade Shows
Vishay History
Products A-Z
Company Info:   Press ·  Investors ·  Contacts ·  More...
Privacy & Legal · Your Account