VishayOne of the world's largest manufacturers of discrete semiconductors and passive components
Vishay ProductsVishay ProductsCompany InfoCompany InfoCompany Info
Company Info:Press Room:2007 Releases:Web Tension Transducers and Web Tension Transmitters from Vishay Systems
For more information:
Media contact: Marti Spalding, Vishay Measurements Group
phone 1.919.365.3800  fax 1.919.365.3945  e-mail marti.spalding@measurementsgroup.com

Technical contact: Don Andres, Vishay Systems
phone 1.781.298.2277  fax 1.781.762.3988  e-mail donald.andres@vishay.com
 

Web Tension Transducers and Web Tension Transmitters from Vishay Systems to Support Efforts of Canadian Forest Sector Research Institute

Equipment Will Enable Paprican to Test and Develop New Papermaking Processes

MALVERN, PENNSYLVANIA — June 29, 2007 — Vishay Intertechnology, Inc. (NYSE: VSH) announces the successful installation of two web tension systems at the pilot papermaking machine operated by Paprican, which is part of FPInnovations, one of the world’s largest forest sector research institutes. Each of the two web tension systems includes two Vishay Systems model HTU transducers and one model LCt-104 signal conditioner/transmitter. The pilot papermaking machine, located in Pointe-Claire, Quebec, Canada, is used to test and develop new papermaking processes. Vishay Systems, which includes the Vishay BLH and Vishay Nobel brands, is a leading manufacturer of equipment and systems for force measurement, process weighing, and on-board weighing.

Vishay Systems installed the equipment as part of an agreement with Paprican. Although the agreement covers an initial three-year period, the Vishay Systems equipment could remain in place for 25 to 30 years, depending on ongoing performance of the equipment and of the papermaking machine.

Each of the model HTU web tension transducers has a dual-axis design that measures horizontal and vertical forces, which enables the measurement of resultant force in any direction. It handles capacities from 2,000 pounds to 20,000 pounds (9 kN to 89 kN), is functional to 250 °F (121 °C), is sealed to meet IP67 requirements, and has a low profile that enables direct load cell replacement. More information is available at http://www.vishay.com/doc?12192.

Each of the model LCt-104 multi-zone web tension transmitters can handle inputs from two HTUs, or one tension zone, to ensure maximum operating speeds without felt breakage. Each zone is measured with 750,000-count resolution and produces a corresponding high-resolution output of 4 mA to 20 mA. The model LCt-104 web tension transmitter features 100 % digital calibration with no dead-weight loading and no strapping required. Interface options include Allen-Bradley Remote I/O, Modbus, DeviceNet, and Profibus. More information is available at http://www.vishay.com/doc?12151.

The equipment installed by Vishay Systems measures and controls the tension in the forming section of the Paprican papermaking machine. The forming section is where paper pulp is jetted onto a continuous fabric belt. The papermaking machine has multiple belts that are pressed together to extract water from the pulp. The Paprican machine is used to test and develop new papermaking processes. Good measurement and control is critical in the forming section.

The environment is harsh, so many sensor technologies will not survive. The Vishay Systems equipment will allow Paprican to control web tension and ultimately optimize the papermaking process.

About Paprican
Paprican, the Pulp and Paper Research Institute of Canada, is a leading not-for-profit research and technology institute that provides valuable technology transfer and cost-competitive research addressing both the short-term and strategic needs of its Members. It has been in business for more than 80 years. Its research programs are driven by the high-priority technical issues of the industry such as product quality and value, cost competitiveness, environment, and sustainability. It also offers results-oriented services to Members and partners, as well as customers from various industries. Internationally recognized for excellence, Paprican operates laboratories in Quebec and British Columbia, and is well positioned to offer services to the global pulp and paper industry. Paprican is part of FPInnovations. Paprican can be found on the Internet at http://www.paprican.ca.

About Vishay Systems
Vishay Systems is a division of Vishay Measurements Group. Vishay Measurements Group develops, manufactures, and markets components, instruments, and systems for a wide variety of test and measurement applications. Vishay strain gage products include electrical resistance strain gages for both stress analysis testing and transducer manufacturing applications, as well as strain gage instrumentation. Vishay PhotoStress® coatings and instruments use a unique optical process to detect stress and other physical forces. Vishay transducer products include load cells, force transducers, and instruments. Vishay also manufactures, installs, and services systems for weighing and force measurement and control. These include systems with transducers and instruments to control process weighing in food, chemical, and pharmaceutical plants; force measurement systems to control web tension in paper mills, roller force in steel mills, and cable tension in winch controls; on-board weighing systems that are installed in logging and waste-handling trucks; and special scale systems for aircraft weighing and portable truck weighing. Vishay Measurements Group is part of Vishay Intertechnology.

Allen-Bradley is a trademark of Allen-Bradley Co., Inc. Modbus is a trademark of Schneider Automation.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###
 
 
 

Products mentioned:

About Vishay
Brands
Careers
Contacts
Ethics
Investor Relations
Product News
2008 releases
2007 releases
2006 releases
2005 releases
2004 releases
*2003 releases
*2002 releases
*2001 releases
*2000 releases
*1999 releases
Trade Shows
Vishay History
Products A-Z
Company Info:   Press ·  Investors ·  Contacts ·  More...
Privacy & Legal · Your Account