Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

Vishay Releases New HE3 Wet Tantalum High-Energy Capacitor With Ultra-High Capacitance Range of 3300 μF to 72000 μF

Device Utilizes SuperTan® Technology to Provide Low ESR of 0.035 Ω


070709he3

Products mentioned:

HE3
For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

This release in:

MALVERN, PENNSYLVANIA — July 9, 2007 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced the release of a new wet tantalum high-energy capacitor that offers the highest capacitance of any similar device on the market. The HE3 features a unique case design with SuperTan® technology for improved reliability and performance in high-energy applications.

Optimized for energy-storage and pulse-power applications in high-reliability avionics and military devices, Vishay’s HE3 is housed in an all tantalum, hermetically sealed case, and is manufactured to withstand high stress and hazardous environments.

The design features a unique double seal for improved reliability and performance, while providing a capacitance range of 3300 μF to 72000 μF, the highest capacitance per unit volume of any wet tantalum capacitor.

The HE3 represents a major breakthrough in wet tantalum capacitor technology by utilizing Vishay’s proven SuperTan hybrid cathode technology in combination with industry-leading anode designs. Its ESR is a very low 0.035 Ω at +25 °C and 1 kHz.

The new capacitor operates over a temperature range of - 55 °C to + 85 °C. It offers a ±20 % standard capacitance tolerance at 120 Hz and + 25 °C, with tolerances of ±10 % also available.

Samples and production quantities of the new HE3 wet tantalum high-energy capacitor will be available in June 2007, with lead times of approximately 8 to 10 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###
Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword