VishayOne of the world's largest manufacturers of discrete semiconductors and passive components
Vishay ProductsVishay ProductsCompany InfoCompany InfoCompany Info
Company Info:Press Room:2007 Releases:Vishay's New Surface-Mount Ambient Light Sensing Photodiodes
For more information:
Media contact: e-mail bob.decker@wallstcom.com
Sales contact: http://www.vishay.com/photo-detectors/sales
 

Vishay’s New Surface-Mount Ambient Light Sensing Photodiodes Are Industry’s First Qualified to Automotive Standard AEC-Q101; Feature Linear Response to Illuminance from 0.1 lux to 100 klux

MALVERN, Pa. — August 24, 2007 — Vishay Intertechnology, Inc. (NYSE: VSH) is broadening its Optoelectronics portfolio with the introduction of the first ambient light sensing photodiodes qualified to the AEC-Q101 standard, a reliability test qualification procedure for discrete semiconductors published by the Automotive Electronics Council.

A key component for automotive body control and passenger safety applications, ambient light sensors allow electronic systems to detect and respond to light in a manner similar to the human eye, eliminating the need for manual adjustments and reducing power consumption. They are typically used to turn on, turn off, or adjust features as a convenience, to conserve battery power, or to provide added safety. Their automotive applications include rain, light, and tunnel sensors; brightness control for dashboard and navigation displays; and automatically turning on the headlights at dusk.

The new TEMD6010FX01 and TEMD5510FX01 use Vishay’s exclusive infrared filtering epoxy technology to match the spectral sensitivity of the human eye with minimal sensitivity to light beyond the visible range. They also provide the benefit of having a closely similar response to either incandescent or fluorescent light, for which the TEMD6010FX01 and TEMD5510FX01 deliver excellent response ratios of 1.3 and 1.4 respectively. For comparison, a standard silicon infrared photo diode has a response ratio of 10.

The TEMD6010FX01 and TEMD5510FX01 provide a linear response to illuminance from 0.1 lux to 100 klux with good lot-to-lot repeatability over the extended operating temperature range of −40 °C to +100 °C. Lot-to-lot repeatability may allow customers to eliminate calibration steps in their manufacturing process. Competing sensors are unable to match this linear response at temperature extremes, particularly above +85 °C.

The new sensors join Vishay’s existing portfolio of ambient light sensing photo transistors, which are also qualified to the AEC-Q101 standard. They are RoHS-compliant, free of halogens, and compatible with lead (Pb)-free soldering. Samples are available now with lead times of six weeks.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

 
Photodiodes
 

Products mentioned:

 

This release in:

About Vishay
Brands
Careers
Contacts
Ethics
Investor Relations
Product News
2009 releases
2008 releases
2007 releases
2006 releases
2005 releases
2004 releases
*2003 releases
*2002 releases
*2001 releases
*2000 releases
*1999 releases
Trade Shows
Vishay History
Products A-Z
Company Info:   Press ·  Investors ·  Contacts ·  More...
Privacy & Legal · Your Account