VishayOne of the world's largest manufacturers of discrete semiconductors and passive components
Vishay ProductsVishay ProductsCompany InfoCompany InfoCompany Info
Company Info:Press Room:2007 Releases:Vishay Releases New High-Speed 1 Form A Solid-State Relay
For more information:
Media contact: e-mail bob.decker@wallstcom.com
Sales contact: http://www.vishay.com/solid-state-relays/sales
 

Vishay Releases New High-Speed 1 Form A Solid-State Relay With 800-µs Turn-On/Turn-Off Times and Low 0.25-Ω On-Resistance

MALVERN, Pa. — September 5, 2007 — Vishay Intertechnology, Inc. (NYSE: VSH) today released a new 1 Form A solid-state relay offering designers fast switching speeds and low on-resistance for a variety of test and measurement and industrial applications.

The VO14642AT features a fast typical switching speed of 800 µs that provides higher throughput in test equipment, as well as low on-resistance of 0.25 Ω that permits the use of multiple relays in applications needing low power consumption and heat dissipation. The relay is rated for a high 2-A DC maximum load current, and a load voltage of 60 V.

An optically isolated device, the VO14642AT provides 5300 V of input-to-output isolation. The relay offers clean, bounce-free switching and is TTL/CMOS-compatible. Available in tape and reel packing, the device features pure tin leads.

Samples of the new VO14642AT 1 Form A solid-state relay are available now. Production quantities will be available in August 2007, with lead times of four to six weeks for large orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

 
VO14642AT
 

Products mentioned:

 

This release in:

About Vishay
Brands
Careers
Contacts
Ethics
Investor Relations
Product News
2008 releases
2007 releases
2006 releases
2005 releases
2004 releases
*2003 releases
*2002 releases
*2001 releases
*2000 releases
*1999 releases
Trade Shows
Vishay History
Products A-Z
Company Info:   Press ·  Investors ·  Contacts ·  More...
Privacy & Legal · Your Account