VishayOne of the world's largest manufacturers of discrete semiconductors and passive components
Vishay ProductsVishay ProductsCompany InfoCompany InfoCompany Info
Company Info:Press Room:2007 Releases:Vishay’s New SMNZ Ultra-High-Precision Z-Foil Four-Resistor Network
For more information:
Media contact: e-mail andrew.post@vishay.com
Sales contact: http://www.vishay.com/resistor-networks/metal-foil/sales
 

Vishay’s New SMNZ Ultra-High-Precision Z-Foil Four-Resistor Network Combines Typical TCR Tracking of 0.1 ppm/°C, PCR Tracking of 5 ppm at Rated Power, Tight Tolerance Match of 0.01 %, and Electrostatic Discharge (ESD) Rating Above 25,000 V

Improved Device Features Load Life Stability of ±0.005 % and Rise Time of 1 ns Without Ringing

MALVERN, Pa. — September 19, 2007 —Vishay Intertechnology, Inc. (NYSE: VSH) today announced the new SMNZ ultra-high-precision Z-Foil four-resistor network, which provides a low absolute TCR of ±0.05 ppm/°C from 0 °C to +60 °C and ±0.2 ppm/°C from −55 °C to +125 °C, an excellent PCR tracking ("ΔR due to self heating") of 5 ppm at rated power, a tolerance match of 0.01 %, a load life ratio stability of 0.005 %, and is available for quick delivery through Vishay’s Fastlane Prototype Service (Foil@vishay.com).

The new SMNZ resistor network is built on Vishay’s breakthrough "Z-foil" technology, which provides a significant reduction of the resistive component’s sensitivity to ambient temperature variations (TCR) and applied power changes (PCR). Z-Foil improves stability by an order of magnitude compared to any other resistor technology, allowing designers to guarantee a high degree of accuracy in fixed-resistor applications.

The SMNZ resistor network combines four independent Bulk Metal® Z-Foil resistors in a single, surface-mount JEDEC MS-012 package with a 50-mil lead pitch. A large variety of resistance ratios is available. Offering better performance and more efficient use of board space than discrete resistors and matched sets, the SMNZ can be used independently or as divider pairs.

Applications for the new SMNZ resistor networks will include instrumentation and differential amplifiers, bridge networks, radio arms in bridge circuits, medical and test equipment, and military and aerospace systems.

The SMNZ device has a load-life stability of ±0.005 % for 2000 hours at 70 °C; a resistance range of 100 Ω to 10 kΩ per resistor; a power rating of 0.4 W (or 0.1 W per resistor) at 70 °C; and current noise less than -40 dB. It offers a fast rise time of 1.0 ns without ringing and features a non-inductive, non-hot-spot design. The SMNZ device offers the utmost in ESD immunity, withstanding electrostatic discharges exceeding 25 kV, for increased reliability.

Samples and production quantities of the SMNZ resistor network are available now via Vishay’s Fastlane Prototype Service, with lead times from two to five days for prototype samples and six weeks for production orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Bulk Metal is a registered trademark of Vishay Intertechnology, Inc.

 
SMNZ
 

Products mentioned:

 

This release in:

About Vishay
Brands
Careers
Contacts
Ethics
Investor Relations
Product News
2008 releases
2007 releases
2006 releases
2005 releases
2004 releases
*2003 releases
*2002 releases
*2001 releases
*2000 releases
*1999 releases
Trade Shows
Vishay History
Products A-Z
Company Info:   Press ·  Investors ·  Contacts ·  More...
Privacy & Legal · Your Account