VishayOne of the world's largest manufacturers of discrete semiconductors and passive components
Vishay ProductsCompany Info
Company Info:Press Room:2007 Releases:Vishay’s New DSMZ Ultra-High-Precision Z-Foil Surface-Mount Voltage Divider
For more information:
Media contact: e-mail andrew.post@vishay.com
Sales contact: http://www.vishay.com/resistor-networks/metal-foil/sales
 

Vishay’s New DSMZ Ultra-High-Precision Z-Foil Surface-Mount Voltage Divider Combines Typical TCR Tracking of <0.1 ppm/°C (0 °C to +60 °C), PCR Tracking of 5 ppm at Rated Power, Tolerance Match of ±0.01 %, and Electrostatic Discharge (ESD) Rating Above 25,000 V

MALVERN, Pa. — October 19, 2007 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced the new DSMZ ultra-high-precision Z-Foil surface-mount voltage divider, which features TCR of ±0.05 ppm/°C from 0 °C to +60 °C and ±0.2 ppm/°C from −55 °C to +125 °C, PCR tracking (“ΔR due to self heating“) of 5 ppm at rated power, tolerance match of ±0.01 %, and load life stability of ±0.005 %.

The new DSMZ voltage divider is built on Vishay’s breakthrough “Z-based“ foil technology, which outperforms all other resistor technologies available today for applications that require ultra-high precision and stability. Greatly reducing the resistive component’s sensitivity to ambient temperature variations (TCR) and applied power changes (PCR), Z-Foil improves stability by an order of magnitude compared to any other resistor technology, allowing designers to guarantee a high degree of accuracy in fixed-resistor applications.

The DSMZ voltage divider provides a matched pair of Bulk Metal® Z-Foil resistors in a single, surface-mount package with dimensions of 4.06 mm by 2.69 mm and a height profile of 1.60 mm. Device features include a load-life stability of ±0.005 % for 2000 hours at 70 °C; a resistance range of 100 Ω to 10 kΩ per resistor; a power rating of 0.05 W per resistor at 70 °C; current noise less than -40 dB; and can withstand electrostatic discharges (ESD) of 25,000 V. The DSMZ offers a fast rise time of 1 to 10 ns (depending on resistance values) without ringing and features a non-inductive, non-hot-spot design.

Applications for the new DSMZ voltage divider will include instrumentation and differential amplifiers, bridge networks, radio arms in bridge circuits, medical and test equipment, and military and aerospace systems. Offering better performance and more efficient use of board space than discrete resistors and matched pairs, the DSMZ is also available in custom versions to meet non-standard technical and application requirements.

Samples and production quantities of the DSMZ voltage divider are available now via Vishay’s Fastlane Prototype Service, with lead times from two to five days for prototype samples and six weeks for production orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Bulk Metal is a registered trademark of Vishay Intertechnology, Inc.

 
DSMZ
 

Products mentioned:

 

This release in:

About Vishay
Brands
Careers
Contacts
Ethics
Investor Relations
Product News
2008 releases
2007 releases
2006 releases
2005 releases
2004 releases
*2003 releases
*2002 releases
*2001 releases
*2000 releases
*1999 releases
Trade Shows
Vishay History
Products A-Z
Company Info:  Press ·  Investors ·  Contacts ·  More...
Privacy & Legal · Your Account