VishayOne of the world's largest manufacturers of discrete semiconductors and passive components
Vishay ProductsVishay ProductsCompany InfoCompany InfoCompany Info
Company Info:Press Room:2008 Releases:Vishay’s 3-V Infrared Receiver Series
For more information:
Media contact: e-mail bob.decker@wallstcom.com
Sales contact: http://www.vishay.com/ir-receiver-modules/
 

Vishay’s 3-V Infrared Receiver Series Offers Enhanced Sensitivity, 70 % Reduction in Operating Current, Broader 2.5-V to 5.5-V Power Supply Range, and Improved EMI and ESD Immunity

MALVERN, Pa. — Jan. 11, 2008 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced that it is upgrading the performance of its 3-V infrared receivers with a new-generation IC that doubles the sensitivity of the device under low-light conditions.

The IC is one of the major determinants of performance in an IR receiver, along with the photo diode and the optical package itself. Sensitivity directly affects the range of a receiver, and is critically important in most infrared receiver applications.

Further improvements resulting from the new IC include a 70 % reduction in device operating current, to 0.35 mA; a broader power supply range of 2.5 V to 5.5 V; and greatly improved immunity to EMI and ESD.

Beginning this month the new IC will become a standard feature of all Vishay 3-V and 5-V infrared receivers in through-hole packages. The upgraded devices can be identified on the Vishay Web site by their part numbers beginning with TSOP3. (except SMD packages [TSOP36.]) and by the word .New. in the datasheet title.

A complete listing of Vishay.s infrared receiver products is available at http://www.vishay.com/ir-receiver-modules/.

No price increase is planned for the new series receivers, which effectively translates into an improved price / performance device for Vishay customers.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

 
3-V Infrared Receivers
 

This release in:

About Vishay
Brands
Careers
Contacts
Ethics
Investor Relations
Product News
2008 releases
2007 releases
2006 releases
2005 releases
2004 releases
*2003 releases
*2002 releases
*2001 releases
*2000 releases
*1999 releases
Trade Shows
Vishay History
Products A-Z
Company Info:   Press ·  Investors ·  Contacts ·  More...
Privacy & Legal · Your Account