English   日本語 (Japanese)   简体中文 (Chinese)   
VishayOne of the world's largest manufacturers of discrete semiconductors and passive components
Vishay ProductsVishay ProductsCompany InfoApplicationsCompany Info
Company Info:Press Room:2008 Releases:Vishay Offers Two Quad ESD Diode Protection Arrays
For more information:
Media contact:  E-mail:  bob.decker@wallstcom.com
Sales contact:  http://www.vishay.com/diodes/protection-tvs-esd/sales
 

Vishay Offers Two Quad ESD Diode Protection Arrays in New Ultra-Compact LLP1010-5L Package With 1-mm by 1-mm Footprint and Low 0.4-mm Profile for Board Space Savings

Devices Feature Low Load Capacitance of 6.5 pF and 12 pF, and Maximum Working Ranges of 5 V and 9 V

MALVERN, Pa. — Jan. 23, 2008 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced the release of two low-capacitance, quad ESD diode protection arrays in the tiny new LLP1010-5L package using environmentally friendly “green” molding compound.

With a compact 1-mm by 1-mm footprint and an extremely low 0.4-mm profile, the VESD05A4A-HS4 and VESD09A4A-HS4 diode protection arrays are designed to save board space and provide 4-line ESD data port protection in space-limited mobile electronics, such as portable gaming systems, MP3 players, and cell phones.

The two devices differ by their maximum working range, low load capacitance, surge current, and low typical leakage current. Both diodes provide transient protection for four data lines as per IEC 61000 4 2 (ESD) at ±15 kV (contact discharge) and ±20 kV (air discharge). The lead (Pb)-free devices are compliant with RoHS 2002/95/EC and WEEE 2002/96/EC.

Diode Protection Array Specification Table

Part number Working range Capacitance Surge current Typ. leakage current
VESD05A4A-HS4 5 V 12 pF >2.5 A <1 µA at 5 V
VESD09A4A-HS4 9 V 6.5 pF >1.5 A <0.5 µA at 9 V

Samples of the new quad ESD diode arrays in the compact LLP1010-5L package will be available in Q4 2007. Production quantities will be available in Q1 2008, with lead times of 10 weeks for large orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

 
Quad ESD
 

Products mentioned

 

This release in:

About Vishay
Brands
Careers
Contacts
Ethics
Investor Relations
Product News
2010 releases
2009 releases
2008 releases
2007 releases
2006 releases
2005 releases
2004 releases
*2003 releases
*2002 releases
*2001 releases
*2000 releases
*1999 releases
Terms and Conditions of Sale
Trade Shows
Vishay History
Products A-Z
Company Info:   Press ·  Investors ·  Contacts ·  More...
Privacy & Legal · Your Account