VishayOne of the world's largest manufacturers of discrete semiconductors and passive components
Vishay ProductsVishay ProductsCompany InfoCompany InfoCompany Info
Company Info:Press Room:2008 Releases:New Vishay Sfernice PE60
For more information:
Media contact: e-mail andrew.post@vishay.com
Sales contact: http://www.vishay.com/resistors-variable/potentiometers/sales
 

New Vishay Sfernice PE60 is Industry’s First Power Panel Potentiometer With a Cermet Element to Offer a Power Rating of 6 W at 50 °C

Device Offers Resistance Ranges from 1 Ω to 1 MΩ and Dielectric Strength of 2500 VRMS in Compact, Fully Sealed Package

MALVERN, Pa. — Feb. 1, 2008 — Vishay Intertechnology Inc. (NYSE: VSH) today announced the industry’s first power panel potentiometer with a cermet element to feature a 6-W power rating at 50 °C.

With US and EU bushing threads and a fully sealed package, the PE60 is intended for industrial and aeronautic control panel and heavy-duty control applications in end products including cockpits, trucks and tractors, HVAC systems, welding machines, tooling machines, field and mine equipment, and water-resistant equipment.

Offering a compact 25-mm diameter, the new Vishay Sfernice device is smaller when compared to other panel potentiometers. Its cermet element provides better stability than carbon elements, while its strong dielectric (2500 VRMS), and non-inductive design offer greater robustness. Custom shafts are available in accordance to drawings supplied by customers.

With resistance ranges from 1 Ω to 1 MΩ, the potentiometer offers a low 3 % typical contact resistance variation and 1 % typical end resistance. The device features a standard ±20 % tolerance, with tolerances of 5 % and 10 % available on request. The PE60 provides a maximum operating torque of 4.3 oz.-inch, and an end stop torque of 6 lb.-inch.

An operating temperature range of −55 °C to +125 °C ensures reliable operation even in extreme environments. The device’s electrical performance is in accordance with CECC 41 000.

Samples and production quantities of the PE60 are available now, with lead times of eight to 10 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

 
PE60
 

Products mentioned:

 

This release in:

About Vishay
Brands
Careers
Contacts
Ethics
Investor Relations
Product News
2008 releases
2007 releases
2006 releases
2005 releases
2004 releases
*2003 releases
*2002 releases
*2001 releases
*2000 releases
*1999 releases
Trade Shows
Vishay History
Products A-Z
Company Info:   Press ·  Investors ·  Contacts ·  More...
Privacy & Legal · Your Account