Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

Vishay’s New Four-, Six-, and Eight-Channel EMI Filters Offer Capacitance of 20 pF and 40 pF, With Typical Cut-Off Frequencies of 130 MHz and 240 MHz

Devices Feature LLPXX13 Leadless Package With Low Profile of 0.6 mm for Board Space Savings


For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

This release in:

MALVERN, Pa. — Feb. 06, 2008 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced the release of six new four-, six-, and eight-channel EMI filters in ultra-compact LLPXX13 leadless packages.

With a low profile of 0.6 mm, the new VEMI filter series is designed to save board space and provide ESD protection in portable electronics for mobile computing, mobile communication, consumer, industrial, and medical applications.

The new filters include the four-channel VEMI45AB-HNH and VEMI45AC-HNH, the six-channel VEMI65AB-HCI and VEMI65AC-HCI, and the eight-channel VEMI85AB-HGK and VEMI85AC-HGK. Delivering high-quality filtering, the new devices feature typical cut-off frequencies of 130 MHz and 240 MHz, a resistance of 100 Ω, and load capacitances of 20 pF and 40 pF. Low leakage current helps to prolong battery life.

The VEMI45AB-HNH, VEMI65AB-HCI, and VEMI85AB-HGK devices provide transient protection for data lines as per IEC 61000 4 2 (ESD) at ± 25 kV and ± 18 kV (air and contact discharge) and IEC 61000 4 5 (lightning) from 4 A (tp = 8/20μs). The VEMI45AC-HNH, VEMI65AC-HCI, and VEMI85AC-HGK devices provide transient protection for data lines as per IEC 61000 4 2 (ESD) at ±12 kV and ± 10 kV (air and contact discharge) and IEC 61000 4 5 (lightning) from 2 A (tp = 8/20μs). All six devices are compliant with RoHS 2002/95/EC and WEEE 2002/96/EC.

New EMI Filter Arrays In Ultra-Compact LLPXX13 Leadless Package: Summary Table

Part Channels Typ. input capacitance
(pF)
Line resistance
(Ω)
Typ. cut-off frequency
(MHz)
Package type
VEMI45AB-HNH 4 40 100 130 LLP1713-9L
VEMI45AC-HNH 4 20 100 240 LLP1713-9L
VEMI65AB-HCI 6 40 100 130 LLP2513-DL
VEMI65AC-HCI 6 20 100 240 LLP2513-DL
VEMI85AB-HGK 8 40 100 130 LLP3313-HL
VEMI85AC-HGK 8 20 100 240 LLP3313-HL

Samples and production quantities of the new EMI filters are available now, with lead times of eight to 10 weeks for large orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword