English   日本語 (Japanese)   简体中文 (Chinese)   
VishayOne of the world's largest manufacturers of discrete semiconductors and passive components
Vishay ProductsVishay ProductsCompany InfoApplicationsCompany Info
Company Info:Press Room:2008 Releases:Vishay Releases New VLMW611.. and VLMW621.. Series
For more information:
Media contact:  E-mail:  bob.decker@wallstcom.com
Sales contact:  http://www.vishay.com/leds/sales
 

Vishay Releases New VLMW611.. and VLMW621.. Series of Warm White Power SMD LEDs in CLCC-6 and CLCC-6 Flat Package With Industry’s Lowest Profile of 0.9 mm

Devices Utilize InGan Technology to Offer Luminous Intensity Range of 1800 mcd to 7100 mcd, and Low Resistance of 40 K/W and 50 K/W

MALVERN, Pa. — March 12, 2008 — Vishay Intertechnology, Inc. (NYSE: VSH) today released two new series of warm white power SMD LEDs that utilize InGan technology to offer low resistance and high optical power. The VLMW611.. series is offered in the CLCC-6 package, while the VLMW621.. series features the CLCC-6 flat package, which offers an industry-low height profile of 0.9 mm.

Among the most robust and light-efficient products on the market, the devices’ ceramic packages make them the ideal light source in applications where careful thermal management is essential. Their low thermal resistance allows these devices to handle the additional current drive needed for maximum light output while maintaining a long service life of up to 50,000 hours.

The new LEDs are optimized for backlighting and illumination in automotive and transport, consumer, and general applications. Typical end products include handheld mobile devices, such as mobile phones and PDAs; instrument panels; marker lights; advertising displays; household appliances, such as refrigerators, washers, and driers; and bicycle lamps.

All devices have a 140-mA forward current, with a 4.3-V maximum forward voltage and 650-mW power dissipation. They provide an optical efficiency of 24 lm/W and an ESD-withstand voltage up to 1 kV according to JESD22-A114-B.

The LEDs offer a 60° half-intensity angle, and are compatible with IR-reflow solder processes according to CECC 00802 and J-STD-020C. The devices are automotive qualified to AEC-Q101 and comply with RoHS 2002/95/EC and WEEE 2002/96/EC. Preconditioned according to JEDEC Level 4 standards, the CLCC-6 and CLCC6 flat packages are lead (Pb)-free and RoHS-compliant.

Device Specification Table

LED Series VLMW611.. VLMW621..
Luminous intensity range 1800 mcd to 7100 mcd 1800 mcd to 7100 mcd
Luminous Flux 5400 mlm to 22300 mlm 5400 mlm to 22300 mlm
Thermal resistance junction/pin 50 K/W 40 K/W
Thermal resistance junction/ambient 100 K/W 90 K/W
Package SMD CLCC-6 SMD CLCC-6 flat

Samples and production quantities of the new VLMW611.. and VLMW621.. power SMD LEDs are available now, with lead times of six weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

 
VLMW62...
 

Products mentioned

 

This release in:

About Vishay
Brands
Careers
Contacts
Ethics
Investor Relations
Product News
2010 releases
2009 releases
2008 releases
2007 releases
2006 releases
2005 releases
2004 releases
*2003 releases
*2002 releases
*2001 releases
*2000 releases
*1999 releases
Terms and Conditions of Sale
Trade Shows
Vishay History
Products A-Z
Company Info:   Press ·  Investors ·  Contacts ·  More...
Privacy & Legal · Your Account