Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

New 30-V TrenchFET Power MOSFET with Industry-Best Maximum 2.25-Milliohm On-Resistance at a 4.5-V Gate Drive Voltage is First Device in Vishay Siliconix TrenchFET® Gen III Family

Device Also Features Industry-Best On-Resistance Times Gate Charge FOM of 98 Milliohms-Nanocoulombs


Si7192DP

Products mentioned:

Si7192DP
For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

This release in:

MALVERN, Pa. — Mar. 26, 2008 — The first device in a new third-generation TrenchFET® power MOSFET family offering record-breaking specifications for on-resistance and on-resistance times gate charge was released today by Vishay Intertechnology, Inc. (NYSE: VSH).

The new TrenchFET Gen III Si7192DP, an n-channel device in the PowerPAK® SO-8 package, features maximum on-resistance of 2.25 milliohms at a 4.5-V gate drive voltage. On-resistance times gate charge, a key figure of merit (FOM) for MOSFETs in dc-to-dc converter applications, is 98, a new industry record for any VDS = 30V, VGS = 20 V device in an SO-8 footprint. Compared to the closest competing devices optimized for low conduction losses and low switching losses respectively, these represent the best available specifications on the market. Lower on-resistance and lower gate charge translate into lower conduction and switching losses respectively.

The Vishay Siliconix Si7192DP will be used as the low-side MOSFET in synchronous buck converters and in secondary synchronous rectification and OR-ing applications. Its low conduction and switching losses will enable more power-efficient and space-efficient designs for voltage regulator modules (VRMs), servers, and a wide range of systems using point-of-load (POL) power conversion.

Siliconix was the industry.s first supplier to introduce Trench power MOSFETs. The company.s TrenchFET IP includes numerous patents, including fundamental technology patents dating from the early 1980s. Each new generation of TrenchFET technology yields products that raise the bar for power MOSFET performance in a wide range of computing, communications, consumer electronics, and many other applications.

Samples and production quantities of the Si7192DP are available now, with lead times of 10 to 12 weeks for large orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

TrenchFET and PowerPAK are registered trademarks of Siliconix incorporated

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword