Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

Vishay Releases New 20-V P-Channel TrenchFET® Power MOSFET in MICRO FOOT® Chipscale Package With Industry’s Thinnest Profile of 0.59-mm

Si8441DB Combines 1.5-mm by 1-mm Footprint Area With an On-Resistance Rating at 1.2-V VGS


Si84x1DB

Products mentioned:

Si8441DB
Si8451DB
For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

This release in:

MALVERN, PENNSYLVANIA — April 9, 2008 — To address the need for smaller components in portable devices, Vishay Intertechnology, Inc. (NYSE: VSH) today released a new 20-V p-channel TrenchFET® power MOSFET in a MICRO FOOT® chipscale package with the industry’s lowest profile and on-resistance for this device type.

The Vishay Siliconix Si8441DB offers an ultra-compact 0.59-mm profile and a footprint area of 1.5 mm by 1 mm. It is also the first device of its kind of offer an on-resistance rating at 1.2 V. Typical applications for the new device will include load switching and battery protection in portable devices such as cell phones, PDAs, digital cameras, MP3 players, and smart phones.

The Si8441DB offers a low on-resistance range from 0.600 Ω at 1.2-V VGS to 0.080 at 4.5-V VGS, with a maximum gate-source voltage of ±5 V. The low on-resistance rating at 1.2 V reduces the need for level shift circuitry, thus saving space in portable electronics designs.

Also released today, in the same MICRO FOOT package, was the 20-V p-channel Si8451DB. Rated for a maximum gate-to-source voltage of 8 V, on-resistance for the Si8451DB ranges from 0.200 Ω at 1.5 V to 0.080 at 4.5 V, the best such values ever achieved for a device with these voltage ratings.

As portable electronics become more compact, and their functionality increases, the available board space for power management circuitry decreases significantly. To meet consumer expectations for battery run times between charges, designers require smaller MOSFET packages with low power consumption—which is exactly what the Si8441DB and Si8451DB provide.

Samples and production quantities of these new MICRO FOOT chipscale power MOSFETs are available now, with lead times of 10 to 12 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword