VishayOne of the world's largest manufacturers of discrete semiconductors and passive components
Vishay ProductsVishay ProductsCompany InfoCompany InfoCompany Info
Company Info:Press Room:2008 Releases:Vishay Releases New 20-V P-Channel TrenchFET®
For more information:
Media contact: e-mail bob.decker@wallstcom.com
Sales contact: http://www.vishay.com/mosfets/sales
 

Vishay Releases New 20-V P-Channel TrenchFET® Power MOSFET in MICRO FOOT® Chipscale Package With Industry’s Thinnest Profile of 0.59-mm

Si8441DB Combines 1.5-mm by 1-mm Footprint Area With an On-Resistance Rating at 1.2-V VGS

MALVERN, PENNSYLVANIA — April 9, 2008 — To address the need for smaller components in portable devices, Vishay Intertechnology, Inc. (NYSE: VSH) today released a new 20-V p-channel TrenchFET® power MOSFET in a MICRO FOOT® chipscale package with the industry’s lowest profile and on-resistance for this device type.

The Vishay Siliconix Si8441DB offers an ultra-compact 0.59-mm profile and a footprint area of 1.5 mm by 1 mm. It is also the first device of its kind of offer an on-resistance rating at 1.2 V. Typical applications for the new device will include load switching and battery protection in portable devices such as cell phones, PDAs, digital cameras, MP3 players, and smart phones.

The Si8441DB offers a low on-resistance range from 0.600 Ω at 1.2-V VGS to 0.080 at 4.5-V VGS, with a maximum gate-source voltage of ±5 V. The low on-resistance rating at 1.2 V reduces the need for level shift circuitry, thus saving space in portable electronics designs.

Also released today, in the same MICRO FOOT package, was the 20-V p-channel Si8451DB. Rated for a maximum gate-to-source voltage of 8 V, on-resistance for the Si8451DB ranges from 0.200 Ω at 1.5 V to 0.080 at 4.5 V, the best such values ever achieved for a device with these voltage ratings.

As portable electronics become more compact, and their functionality increases, the available board space for power management circuitry decreases significantly. To meet consumer expectations for battery run times between charges, designers require smaller MOSFET packages with low power consumption—which is exactly what the Si8441DB and Si8451DB provide.

Samples and production quantities of these new MICRO FOOT chipscale power MOSFETs are available now, with lead times of 10 to 12 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

 
Si84x1DB
 

Products mentioned:

 

This release in:

About Vishay
Brands
Careers
Contacts
Ethics
Investor Relations
Product News
2008 releases
2007 releases
2006 releases
2005 releases
2004 releases
*2003 releases
*2002 releases
*2001 releases
*2000 releases
*1999 releases
Trade Shows
Vishay History
Products A-Z
Company Info:   Press ·  Investors ·  Contacts ·  More...
Privacy & Legal · Your Account