VishayOne of the world's largest manufacturers of discrete semiconductors and passive components
Vishay ProductsVishay ProductsCompany InfoCompany InfoCompany Info
Company Info:Press Room:2008 Releases:Vishay Releases New TR8 Series of Molded MicroTan™ Tantalum Chip Capacitors
For more information:
Media contact: e-mail andrew.post@vishay.com
Sales contact: http://www.vishay.com/capacitors/solid-tantalum/sales
 

Vishay Releases New TR8 Series of Molded MicroTan™ Tantalum Chip Capacitors with ESR of 0.8 Ω in 0805 Case Size, and Industry’s Lowest ESR of 1.5 Ω for the 0603 Case Size

Devices Offer Capacitance Range of 1.0 µF to 220 µF and Voltage Ratings from 4 WVDC to 16 WVDC for Portable Electronics

MALVERN, PENNSYLVANIA — May 14, 2008 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced the release of the new TR8 series of molded MicroTan™ tantalum chip capacitors that provide ultra-low ESR values of 0.8 Ω (at 100 kHz and 47 µF) in the 0805 case size, and an industry-low 1.5 Ω in the 0603 case size.

Low ESR values, combined with small 0603 and 0805 footprints, allow for greater efficiency in audio filtering and signal processing applications, while requiring less PCB space. The new TR8 capacitors are intended for applications in cell phones, digital cameras, MP3 players, and other portable devices.

Like all series within the MicroTan™ family, the TR8 is fully RoHS-compliant and halogen-free in accordance with Vishay’s commitment to supporting environmentally friendly “green” initiatives. The devices feature lead (Pb)-free, L-shape facedown terminations for better contact to the solder pad than traditional facedown-style terminations. In addition, their rectangular molded case encapsulation helps to streamline PCB assembly.

Capacitance values for the TR8 series range from 1.0 µF to 220 µF, with standard capacitance tolerances of ±10% and ±20%. Voltage ratings range from 4 WVDC to 16 WVDC. The operating temperature range for the devices is -55 °C to +85 °C, or +125 °C with voltage derating.

The capacitors are available in 8-mm tape and reel packaging per EIA-481-1 and 7-in [178-mm] standard reeling per IEC 286-3.

Samples and production quantities of the new TR8 molded MicroTan tantalum chip capacitors are available now, with lead times of 8 to 10 weeks for larger orders. Pricing is available on request.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

 
TR8
 

Products mentioned:

 

This release in:

About Vishay
Brands
Careers
Contacts
Ethics
Investor Relations
Product News
2008 releases
2007 releases
2006 releases
2005 releases
2004 releases
*2003 releases
*2002 releases
*2001 releases
*2000 releases
*1999 releases
Trade Shows
Vishay History
Products A-Z
Company Info:   Press ·  Investors ·  Contacts ·  More...
Privacy & Legal · Your Account