Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

Vishay Releases New Enhanced 10-A to 25-A PowerBridge™ Rectifier Series With 600-V to 1000-V VRRM

Space-Saving Devices Offer More Efficient Performance Than Larger Bridge Products While Reducing Need for Heat Sinks


PowerBridge

Products mentioned:

BU25
BU20
BU15
BU12
BU10
For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

This release in:

MALVERN, PENNSYLVANIA. — May 28, 2008 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced a new series of enhanced high-current-density PowerBridge™ rectifiers with current ratings of 10 A to 25 A and maximum peak reverse voltage ratings of 600 V to 1000 V.

Compared to larger-size bridge rectifiers on the market, the advanced thermal construction of the PowerBridge devices allows heat to dissipate more efficiently. The PowerBridge rectifiers are thus able to provide the same power ratings as larger packages while requiring smaller heat sinks.

The single-phase rectifiers are an optimal bridge package choice for ac-to-dc rectification in switchmode power supplies for desktop PCs, servers, PDP TVs, LCD TVs, audio/video systems, and adaptors for notebook PCs and monitors; power inverters in home appliances such as refrigerators, washing machines, air conditioners, and induction heater systems; and primary rectification circuits for switchmode power supplies in telecommunication systems.

For OEM vendors, the new devices offer compatible package, lead pitch, and pin layouts to conventional GBU packages. This saves time by allowing the same PCB layout to be used for a wide range of bridge rectifier voltage and current ratings. For manual soldering, a +260 °C, 40-second solder dipping process enables high reliability.

Single-Phase Bridge Rectifier Specification Table

Device Maximum peak reverse voltage and forward surge current ratings VF @ IF per chip, TJ
BU25 600-V to 1000-V, 25-A 0.87 V typ. @ 12.5 A, +125 °C
BU20 600-V to 1000-V, 20-A 0.85 V typ. @ 10 A, +125 °C
BU15 600-V to 1000-V, 15-A 0.87 V typ. @ 7.5 A, +125 °C
BU12 600-V to 1000-V, 12-A 0.88 V typ. @ 6 A, +125 °C
BU10 600-V to 1000-V, 10-A 0.88 V typ. @ 5 A, +125 °C

Samples and production quantities of the new PowerBridge rectifiers are available now, with lead times of six weeks for large orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword