|
For more information: Vishay Releases New Enhanced 10-A to 25-A PowerBridge™ Rectifier Series With 600-V to 1000-V VRRMSpace-Saving Devices Offer More Efficient Performance Than Larger Bridge Products While Reducing Need for Heat Sinks
MALVERN, PENNSYLVANIA. — May 16, 2008 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced a new series of enhanced high-current-density PowerBridge™ rectifiers with current ratings of 10 A to 25 A and maximum peak reverse voltage ratings of 600 V to 1000 V. Compared to larger-size bridge rectifiers on the market, the advanced thermal construction of the PowerBridge devices allows heat to dissipate more efficiently. The PowerBridge rectifiers are thus able to provide the same power ratings as larger packages while requiring smaller heat sinks. The single-phase rectifiers are an optimal bridge package choice for ac-to-dc rectification in switchmode power supplies for desktop PCs, servers, PDP TVs, LCD TVs, audio/video systems, and adaptors for notebook PCs and monitors; power inverters in home appliances such as refrigerators, washing machines, air conditioners, and induction heater systems; and primary rectification circuits for switchmode power supplies in telecommunication systems. For OEM vendors, the new devices offer compatible package, lead pitch, and pin layouts to conventional GBU packages. This saves time by allowing the same PCB layout to be used for a wide range of bridge rectifier voltage and current ratings. For manual soldering, a +260 °C, 40-second solder dipping process enables high reliability. Single-Phase Bridge Rectifier Specification Table
Samples and production quantities of the new PowerBridge rectifiers are available now, with lead times of six weeks for large orders.
Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com. This press release refers to products under a trademark (PowerBridge) that has been replaced. These products are now referred to as isoCink+™ products. |