VishayOne of the world's largest manufacturers of discrete semiconductors and passive components
Vishay ProductsVishay ProductsCompany InfoCompany InfoCompany Info
Company Info:Press Room:2008 Releases:New Vishay Siliconix Power MOSFETs in Compact 2-mm by 2-mm PowerPAK® SC-70 Package
For more information:
Media contact: e-mail bob.decker@wallstcom.com
Sales contact: http://www.vishay.com/mosfets/sales
 

New Vishay Siliconix Power MOSFETs in Compact 2-mm by 2-mm PowerPAK® SC-70 Package Offer Half the Size of TSOP-6 With Comparable On-Resistance Down to 11 mΩ

Offering Includes Industry’s First 12-V Devices in This Package Type, and MOSFETs With Industry’s Lowest On-Resistance For Voltage Rating and Package Size

MALVERN, Pa. — May 28, 2008 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced the release of 15 new power MOSFETS in a PowerPAK® SC-70 package measuring 2 mm by 2 mm with a low 0.8-mm profile.

The new offering includes a variety of configurations and voltage ratings for different applications, including single, single plus Schottky, and dual devices, in both n-channel and p-channel, in addition to n- and p-channel complementary pairs. The devices feature voltage ranges between 8 V and 30 V with extremely low on-resistance values down to 0.011 Ω at 4.5 V.

As portable devices become smaller, and as functionality increases, their available board space becomes more limited. Designers are forced to find smaller solutions, while at the same time maintaining low power consumption to keep batteries running as long as possible between charges.

To meet this need, the PowerPAK SC-70 combines the tiny footprint of the SC-70 package with on-resistance comparable to the larger TSOP-6. The result is a solution with very low power consumption in a package that is 50 % smaller than the TSOP-6 and 27 % thinner. In addition to helping the environment by saving energy, the PowerPAK SC-70 is 100 % lead (Pb)-free, halogen-free, and RoHS-compliant, meeting the demands of international legislation for elimination of hazardous substances.

Typical applications for Vishay Siliconix PowerPAK SC-70 MOSFETs will include load switching and battery charging in portable devices such as cell phones, PDAs, digital cameras, and MP3 players, as well as notebook computers, portable HDDs, and miniature motor drives.

The devices released today include the SiA413DJ, which is the industry’s first 12-V single p-channel device in this package size. The SiA913DJ and SiA912DJ are the first 12-V dual p- and n-channel MOSFETs, respectively, while the SiA511DJ is the first 12-V n-channel and p-channel complementary pair.

Several of the devices set new records for on-resistance in the SC-70 footprint. With a rating of 0.056 Ω at 4.5 V, the new SiA421DJ has the lowest on-resistance in the 30-V single p-channel category. At 0.053 Ω, the SiA914DJ offers the industry’s lowest on-resistance for a 20-V dual p-channel MOSFET. Two of the new products features on-board, low-VF Schottky diodes. Rated at 0.053 Ω, the SiA810DJ offers the lowest on-resistance for a 20-V single n-channel plus Schottky device, while the 0.094-Ω SiA811DJ achieves the same distinction for a 20-V single p-channel plus Schottky.

The SiA413DJ and SIA411DJ MOSFETs feature on-resistance ratings down to 1.5-V VGS, enabling low power consumption and saving board space by reducing the need for level shift circuitry. Previously released devices in the PowerPAK SC-70 include the SiA414DJ, SiA417DJ, and SiA419DJ with on-resistance ratings down to 1.2-V VGS. The 0.011-Ω SiA414DJ and 0.023-Ω SiA417DJ are additionally the first devices in this package type with an 8-V breakdown voltage rating.

Complete details on all Vishay Siliconix power MOSFETs in the PowerPAK SC-70 package are available at http://www.vishay.com/mosfets/powerpak-sc-70-package/.

Samples and production quantities of the 15 new power MOSFETS are available now, with lead times of 10 to 12 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

TrenchFET, PowerPAK, and PolarPAK are registered trademarks of Siliconix incorporated

 
Power MOSFETs
 

This release in:

About Vishay
Brands
Careers
Contacts
Ethics
Investor Relations
Product News
2008 releases
2007 releases
2006 releases
2005 releases
2004 releases
*2003 releases
*2002 releases
*2001 releases
*2000 releases
*1999 releases
Trade Shows
Vishay History
Products A-Z
Company Info:   Press ·  Investors ·  Contacts ·  More...
Privacy & Legal · Your Account