![]() |
|
||||||
|
|
|
For more information:
Media contact: e-mail bob.decker@wallstcom.com Sales contact: http://www.vishay.com/mosfets/sales Vishay Releases New 20-V P-Channel TrenchFET® Power MOSFET in MICRO FOOT® Chipscale Package With Industry’s Smallest Footprint of 1.2-mm by 1.0-mmSi8445DB Combines Ultra-Slim Profile of 0.59 mm with Low 0.495-Ω On-Resistance at 1.2-V VGSMALVERN, PENNSYLVANIA — June 18, 2008 — Vishay Intertechnology, Inc. (NYSE: VSH) today released a new 20-V p-channel TrenchFET® power MOSFET in a MICRO FOOT® chipscale package that features the industry’s smallest footprint and on-resistance ratings down to 1.2 V. As portable electronics become more compact, and their functionality increases, the available board space for power management circuitry decreases significantly. To meet consumer expectations for battery run times between charges, designers require smaller MOSFET packages with low power consumption—which is exactly what the new Vishay Siliconix Si8445DB provides. With an ultra-compact 1.2-mm by 1.0-mm footprint, the Si8445DB is 20 % smaller than the industry’s next-smallest device, while offering the same slim 0.59-mm profile. The Si8445DB offers a low on-resistance range from 0.495 Ω at 1.2-V VGS to 0.084 at 4.5-V VGS. The low on-resistance rating at 1.2 V reduces the need for level shift circuitry, thus saving space and power in portable electronics designs. Typical applications for the new device will include low-threshold load switching, charger switching, and battery management in portable devices such as cell phones, PDAs, digital cameras, MP3 players, and smart phones. Samples and production quantities of the new MICRO FOOT chipscale power MOSFET are available now, with lead times of 10 to 12 weeks for larger orders. Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com. ###
TrenchFET and MICRO FOOT are registered trademarks of Siliconix incorporated. | ![]() | ||||
|
|||||
| ||||||