English   日本語 (Japanese)   简体中文 (Chinese)   
VishayOne of the world's largest manufacturers of discrete semiconductors and passive components
Vishay ProductsVishay ProductsCompany InfoApplicationsCompany Info
Company Info:Press Room:2008 Releases:Vishay’s New CSM2512S Bulk Metal® Surface-Mount Power Metal Strip® Resistor
For more information:
Media contact:  E-mail:  andrew.post@vishay.com
Sales contact:  http://www.vishay.com/resistors-discrete/ultra-high-precision/sales
 

Vishay’s New CSM2512S Bulk Metal® Surface-Mount Power Metal Strip® Resistor Offers Improved Load-Life Stability of 0.05 %, Absolute TCR of ±15 ppm/°C, and Tolerance of ±0.1 %

High-Precision Current Sensing Device Features Resistance Values From 10 mΩ and Rated Power to 1 W in a 4-Terminal Kelvin Design

MALVERN, PENNSYLVANIA — June 27, 2008 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced a new high-precision Bulk Metal® surface-mount Power Metal Strip® resistor that features an improved load-life stability of ±0.05 % at +70 °C for 2000 hours at rated power, an absolute TCR of ±15 PPM/°C from −55 °C to +125 °C, +25 °C Ref., and a tolerance of ±0.1 %.

Typical current sensing resistors offer a load-life stability of ≥ 0.5 % through a 1000-hour workload. The improved resistance stability of the CSM2512S makes it ideal for tightened-stability voltage division and precision current sensing applications in switching linear power supplies, power amplifiers, measurement instrumentation, bridge networks, and medical and test equipment. In addition, the CSM2512S complies with EEE-INST-002 (MIL-PRF 55342 and MIL-PRF 49465) for military and space applications.

The CSM2512S’s all-welded construction is composed of a Bulk Metal® resistive element with plated copper terminations. The resistor element is designed to uniformly dissipate power in order to minimize hot spots, and is compatible with the lead material, resulting in a low thermal EMF of 3 µV/°C.

The CSM2512S provides a 1-W power rating and maximum current up to 18 A in a four-terminal Kelvin configuration for increased accuracy. Any value at any tolerance is available within the resistance range of 10 mΩ to 100 mΩ at no additional cost.

Samples and production quantities of the CSM2512S high-precision resistor are available now, with lead times of 72 hours for samples, and three weeks for standard orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Bulk Metal and Power Metal Strip are registered trademarks of Vishay Intertechnology, Inc.

 
CSM2512S
 

Products mentioned

 

This release in:

About Vishay
Brands
Careers
Contacts
Ethics
Investor Relations
Product News
2010 releases
2009 releases
2008 releases
2007 releases
2006 releases
2005 releases
2004 releases
*2003 releases
*2002 releases
*2001 releases
*2000 releases
*1999 releases
Terms and Conditions of Sale
Trade Shows
Vishay History
Products A-Z
Company Info:   Press ·  Investors ·  Contacts ·  More...
Privacy & Legal · Your Account